Slider
The widget is available under designing application pages, drag-and-drop slider to a container. To use the old version, refer to Slider.
. WhenSlider Properties
Field Name | Description |
---|---|
Label | A label name that appears as a header for the slider. |
Source > Input Value | Provide the input data source to receive values for the slider. See Bind Your Data to Plug-ins. |
Minimum Value | Sets the minimum scale value. |
Maximum Value | Sets the maximum scale value. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. |
Target > Output Value | Provide the target data source to send information. |
Label Styling | Formats the label: Font Family, Font Size, and Font Color formats the label text. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |