Pie Chart
The widget is available under designing application pages, drag-and-drop Pie Chart to a container.
. WhenPie Chart Properties
Field Name | Description |
---|---|
Pie Type | Select from the available list of pie charts. |
Source > Data Source | Provide the input data source to receive values for the chart. |
Title | Title name for the chart. |
Subtitle | Subtitle name for the chart. |
Legend | Select the Visible check box if you want to show the chart legend. You can also use the options to position the legend in the chart. |
Show Labels | Select the check box if you want to show labels in the chart. |
Show Tooltips | Select the check box if you want to show tool tips in the chart. |
Show Name | Select the check box if you want to show label name. |
Show Value | Select the check box if you want to show values in the tooltip. |
Show Percentage | Select the check box if you want to show percentages in the tooltip. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |
Note: When exporting a chart to JPEG or PDF at runtime, make sure your browser's zoom is
set to 100% or above.