Breadcrumb
With the GEBreadcrumb plug-in, you can navigate through the asset model.
The purpose of a breadcrumb is to allow you to access an asset's information located anywhere in the asset model hierarchy. A breadcrumb navigation also defines the relationship between different assets in a model.
The breadcrumb navigation is available for all the widgets in Operations Hub. You can navigate in the trend card using breadcrumb.


To use the plug-in in the page designer, drag GEBreadcrumb from to a container on the page.

You must specify these breadcrumb properties:
The breadcrumb is customizable, enabling you to add conditions for display navigation. Refer to Page Components (Classic) for common widget properties.
Breadcrumb Properties
Field Name | Description |
---|---|
Source Asset Context | Select the source (asset name) for an asset context. The selected context
appears as a default breadcrumb view in the end application. This asset name
must exist in your asset
model.![]() |
Target Asset Context | Select the target for an asset context. This target defines where that
output goes on selecting an asset in a breadcrumb, so that it can be fed either
to a query or a global.![]() |
Target Extension Query for Asset Context Properties | Select the target for an extension query. This is a formatted string with
a list of properties that defines the hierarchy of the breadcrumb in the end
application. For example, consider these crumbs in a hierarchy - first is
‘pump’, second is ‘pump pressure’, ‘pump frequency’, ‘pump vibration’, or ‘pump
flow’. ![]() |