Export CIMPLICITY Self-Signed Certificate

Export this certificate that was created when CIMPLICITY was installed on the system.

The certificate is exported and then imported into the Trusted Certificate store on the Operations Hub computer.
  1. Open Windows Run, and enter certmgr.msc.
  2. Go to Trusted Root Certification Authorities > Certificates.
  3. Select the certificate named CIMPLICITY<computer_name><datetime>@SelfsignedRootCA.
  4. Right-click CIMPLICITY self-signed certificate, then select All Tasks > Export.
    The Certificate Export Wizard appears.
  5. Select Next.
  6. When prompted for the Export File Format, select DER encoded binary X.509 (.CER).
  7. Select Next.
  8. Select Browse, enter file name of CIMPLICITY_Self_Signed and choose to save on the Desktop.
  9. Select Next.
  10. Select Finish.