Create Extension Query
This topic describes how to an Extension query.
About this task
Procedure
-
In the main navigation menu, select QUERIES.
The QUERIES workspace appears.
-
Select Add new query.
The New Query window appears.
-
Provide these details:
Field Description Name Enter a name that contains at least one uppercase or lowercase letter. Description Enter a brief description for the query. Type Select Extension. Method Select the type of query you want to create from these options: - Read
- Write
- Add Comment
The Query Parameters and Output Data are loaded based on the method selected for the query.
-
Provide the query parameter values
for the required fields.
- Fixed Value: If this option is selected, the provided value is considered as a fixed value for the field. Fixed value fields are not shown in the application page builder.
- Input Field: If this option is selected, the provided value appears as a default value for the field in the page builder. Any value provided before executing the query overrides the default value.
-
Select
next to the parameters you do not want to include in your query.
To retrieve deleted query parameters and output data, select +Add All Query Params and +Add All Outputs respectively.
-
Save the query.
The extension query is created.