Delete an Application
Delete applications from Operations Hub.
About this task
- When you delete an application, only the application is deleted from Operations Hub. The components used by the application are not deleted.
- You cannot delete an application if it is locked.
- You cannot delete Operations Hub default applications.
Procedure
- In the main navigation menu, select
APPS.The APPS workspace appears.
- In each row containing an application that you want to delete, select the check box.
- In the workspace heading, select , and then select Delete apps.A message appears, asking you to confirm that you want to delete the applications.Tip: Alternatively, in the row containing each application that you want to delete, select , and then select Delete app.
- Select OK.The applications are deleted.