Create a Relationship Between Entities
About this task
Procedure
- In the main navigation menu, select
ENTITIES.The ENTITIES workspace appears.
- Optional: Select the check boxes of the entities for which you want to create a relationship.
- Select DESIGNER.The DESIGNER section appears, displaying all the entities created in the site. If, however, you have selected entities in the previous step, only the selected entities appear. If a relationship exists between two entities, a line connecting them appears.Tip: You can arrange the entities in an order, minimize all entities, maximize all entities, or maximize only the entities in a relationship by selecting Auto Arrange, Minimize All, Maximize All, or Maximize linked Entities respectively.
- Next to each entity for which you want to create a relationship, select .A list of fields in each entity appears.
- Select Add Relationship, and then select a field from the source entity and then the target entity.A relationship is created between the entities. A line connecting both the entities appears.