Import an Application
Import and save applications to Operations Hub.
- In the main navigation menu, select
APPS.The APPS workspace appears.
- Select Import App.A message appears, indicating that if there is already an application or a component with the same name, the imported application or component will contain a new name.
- Proceed to import the application.
-
Navigate to the application (stored as a .zip file) that you want to import,
then select Open.
Important: To avoid system related errors, do not modify original exported zip files and repackage them for import.
-
If the application being imported already exists in Operations Hub with the
same name, select one of the following:
Option Description Duplicate Creates a duplicate copy of the application and imports to Operations Hub. Replace Deletes the existing application in Operations Hub and replaces with the one from the import file. If duplicate data source records are found, you may be asked to confirm before importing the file to Operations Hub. Refer to Handling Duplicate OPC UA Data Sources. - If the system detects that the imported application has widgets/plug-ins eligible for upgrades, then they are automatically updated to their latest versions. See Configure Plug-in Upgrades.