Handling Duplicate OPC UA Data Sources
OPC UA data sources are identified as duplicates if they contain identical server endpoint values.
If duplicate OPC UA data sources are detected during application import, select one of the following:
Option | Description |
---|---|
Use Existing | Maintains the data source record that currently exists in Operations Hub. Does not import the duplicate from the file. |
Replace | Deletes the data source record that currently exists in Operations
Hub. Imports the duplicate from the file to replace the deleted
record. Note: This option is enabled only for duplicate data source
records sharing the same name and endpoint connection value (URI).
Details such as security policy, authentication, etc. may vary in
these records. |
Duplicate Apps in Operations Hub: During import conflict, if you opt for duplicating the application, the relevant data sources are also duplicated.
To resolve any OPC UA data source server endpoint (URI) conflict when duplicating apps:
- Select Use Existing to avoid deleting the existing OPC UA record in Operations Hub. This record will not be imported from the file.
- Select Replace, to replace the existing OPC UA record in Operations Hub with the record from the import file.
Replace Apps in Operations Hub: During import conflict, if you opt for replacing
the application, Operations Hub data source records having the same name as the imported
records, are deleted before being replaced with the imported ones.
Note: Any OPC UA data
source record in Operations Hub that shares the same name with a record from the
import file will get replaced in this scenario. Such records are not considered to
be duplicates.
To resolve any OPC UA data source server endpoint (URI) conflict when replacing apps:
- Select Use Existing to avoid deleting the existing OPC UA record in Operations Hub. This record will not be imported from the file.
- Select Replace, to replace the existing OPC UA record in Operations Hub with the record from the import file.
Note: Duplicate OPC UA data sources that existed in older versions are not removed after
upgrading to 2.1 or later. It is recommended to manually delete such duplicate records,
or modify them to use a unique server endpoint connection.