Access the Trend Chart with Asset Model

  1. Create a data source to connect to the Historian server.
    For instructions, refer to the Data Sources section of the User Guide.
  2. Set up the Historian server.
    For instructions, refer to the Administration section of the User Guide.
  3. Import the model to Operations Hub.
    For instructions, refer to the Administration section of the User Guide.
  4. For the model that you have imported, enable the trendable properties by performing the following properties:
    1. In the Admin workspace, select Visualizations > Designer.
    2. For each data variable that is trendable, select the check box in the Trendable check box.
  5. Access the Historian Analysis application.
    For instructions, refer to the Applications section of the User Guide.
When you navigate to the model, the trend chart plots data based on the selected context.