Configuring Windows User Accounts on the Batch REST Service Computer
The batch widgets send a bearer token to the Batch Rest Service containing the currently
logged in Ophub User account name. This account name must exist on the Batch Rest
Service computer as a local Windows user, or as a domain user.
- If using local Windows user accounts, create the corresponding local Windows user accounts on the Batch REST Service computer that match the Ophub user account names.
- If you are using a domain user, the domain name can be a part of the Operations
Hub user name (for example:
ophubuser@DomainName
). You can also use an Ophub account name without domain as part of the Operations Hub username. For example,ophubadmin
. - If you use an Operations Hub user name without domain, for example
ophubadmin
, the Batch REST Service will first look up this user to see if it is a valid local Windows user on the Batch REST Service computer. If it is not found, then it will look up this user on the Domain used by the computer. The order of the user lookup can be customized with theUAAUserDomainLookupOption
property and is described in more detail the Batch Rest APIreadme.txt
. - As an extra security feature, if the
basicAuthWindowsGroupValidation
property istrue
, the Batch REST Service will validate that this user is a member of thebasicAuthWindowsGroup
. This group is initially set toPROFICY_BATCH_REST_USERS
. If this is set totrue
, then be sure to add the windows user accounts to this Windows User Group.
Use e-Signatures
To use e-Signatures for batch widgets, do the following:
- Create Windows user groups on the Batch REST Service computer that correspond to
the e-Signature Requirement
Performed By
andVerified By
group names in the batch widgets.For example,
Operator
andSupervisor
group names are used in the Batch widgets sample application. - Create Windows users on the Batch REST Service computer and add them to the appropriate Windows user group used for e-Signature. Or if you are using Domain users, add the domain users to the appropriate Windows user groups used for e-Signature.
- Be sure that the Windows User accounts
full name
is not blank. - If using Domain users, be sure to set the
GE Intelligent Platforms Security Server (iSecurity.exe)
Windows Service to run under a Domain user account, and restart this service.