Access the Trend Chart without Asset Model

You can access the trend chart without the asset model (that is, by browsing through the Historian data source directly for use in the trend chart).

Procedure

  1. Create a data source to connect to the Historian server. For instructions, refer to the Data Sources section of the User Guide.
  2. Set up the Historian server. For instructions, refer to the Administration section of the User Guide.
  3. Access the Historian Analysis application. For instructions, refer to the Applications section of the User Guide.
  4. Access the trend chart configuration to select the tags that you want to plot on the trend chart. For instructions, refer to the Widgets section of the User Guide.

Results

Data for the selected tags is plotted on the trend chart.