Inspection Tasks
About Inspection Tasks and Recommendations
Based on the results of an inspection, you might need to suggest that further action be taken. For example, if you inspect an area of a warehouse and notice that the roof is leaking, you may want to suggest that the ceiling tiles be replaced.
You can create a new Inspection Task record that indicates that the ceiling tiles need to be replaced, or you could create an Inspection Recommendation record to record the recommendation to replace the ceiling tiles. Your business processes will dictate whether you should create an Inspection Task record or a Recommendation record. For example, inspectors may need to report all recommendations to a supervisor for approval. The supervisor might then be responsible for approving the recommendation, creating an associated Inspection Task record, and assigning that Inspection Task record to the appropriate inspector.
Additionally, if the Thickness Monitoring license is active and TM Analyses exist for the Equipment records that you analyze in Inspection Management, you can specify that Inspection Task records be updated based upon Thickness Measurement records that you create in Thickness Monitoring. Specifically, the value in the Last Date field in the Inspection Task record will be populated with the value in the Measurement Taken Date field in the Thickness Measurement records that you create via the TM Measurement Data Entry page.
About Generating Inspections for Related Inspection Tasks
After the cost has been estimated for the work associated with all Inspection Tasks for a given Work Pack, you can determine which inspections you will perform and which you will not. You can then create Inspections to represent the approved work that you will perform.
Example: Generating Inspections
For example, suppose a Work Pack includes tasks to inspect all pieces of equipment in a particular system. If you receive an estimate from an inspector that exceeds your budget, you might need to trim the inspection work and inspect only the pieces of equipment whose previous inspections revealed defects.
You can generate Inspections for the Inspection Tasks by:
View Linked Inspection Tasks Details
Procedure
Access the Inspection Tasks Section
Procedure
Create an Inspection Task
Access the Related Records of an Inspection Task
Procedure
About Deferring an Inspection Task
There may be instances when a task cannot be completed by the specified Next Date due to various reasons. In this scenario, APM provides a workflow to request a deferral of the task. The deferral follows a review and approval process allowing an inspector to request the deferral by providing a reason and selecting the desired deferral date. The inspection supervisor can review the request and decide to approve or reject it.
Upon approval of a deferral request, the following fields are updated on the Inspection Task:
- Original Next Date: Updated with the value of the Next Date field on the task. This value is only updated upon the approval of the first deferral within this cycle and is retained until the task is executed.
- Next Date: Updated with the value of the Deferred Date field on the approved Deferral.
- Deferred Next Date Basis: Updated with the ID of the approved Deferral.
- Is Deferred: Updated to true to indicate that a Deferral has been approved for this task.
- Reason: Appended with the value from the Comments field along with the Deferral ID and current date of the approved Deferral.
Multiple Deferral records can be created and approved for a given Inspection Task if required. However, the number of times a task can be deferred is restricted and controlled by the Deferral Configuration for the Inspection Task family.
When there is at least one approved Deferral against a task and the task is either addressed by a completed inspection or the Next Date field is updated with a greater value, the following occurs:
- The Original Next Date, Deferred Next Date Basis, and Is Deferred fields are cleared.
- Any approved Deferrals are moved to the Archived state.
Create a Deferral for an Inspection Task
Before You Begin
Procedure
Access the Deferrals of an Inspection Task
Before You Begin
Ensure that Enable Deferral option is selected for the Inspection Task family in the Deferral Configuration workspace.
Procedure
Delete a Deferral of an Inspection Task
Before You Begin
Ensure that Enable Deferral option is selected for the Inspection Task family in the Deferral Configuration workspace.
Procedure
Manage Deferrals
Procedure
Modify the Date Filter for Inspection Tasks
About This Task
The Underlying Inspection Tasks section can be filtered using the Next Date Filter. Inspection tasks are filtered based on the value in the Task Next Date field. If you do not modify the filter when accessing tasks, the sections may appear to be empty. You can modify the date filters to display the tasks that you want to access. By default, the selected date filter is defined by the administrator, but user preferences take priority once saved.
Procedure
Create an Inspection Report from an Inspection Task
Procedure
Results
- A new Inspection record is created for the specified Inspection Document Type.
- You can now access Inspection Reports.
Delete an Inspection Task
Procedure
About Schematic Visualization of Scope of Work
To aid in performance of inspections, a PDF document that outlines various aspects of the Inspection may be used. You can upload, download, and remove an Inspection Scope Visualization Document from the Scope tab of an Inspection.
View Inspection Scope Visualization Details
Procedure
Upload an Inspection Scope Visualization Document
Procedure
Download an Inspection Scope Visualization Document
Procedure
- Access the Inspection Details section.
- Select Scope tab.
- Select the filename hyperlink within the Inspection Scope Visualization section. The Inspection Scope Visualization Document will automatically be downloaded in your browser.