End-of-Life Features

End-of-Life Features in V5.2.1.0.0

There are no end-of-life features in this release.

Upcoming End-of-Life Features

  • Calibration Management: As part of continuous improvement process, integration of Calibration Management module with Druck calibrators will no longer be supported with the Q3 2025 release. The following Calibrators will reach end of life and will no longer be available with the Q3 2025 release.
    • Druck DPI611
    • Druck DPI612
    • Druck DPI620
    • Druck DPI620G (Genii)
    • Druck DPI620G-IS (Genii)
    • Druck DPI620-IS
  • Life Cycle Cost Analysis: As part of continuous improvement process, Life Cycle Cost Analysis will reach end of life and will be no longer available with the Q3 2025 release.
  • Pipeline Integrity Management: As part of continuous improvement process and lack of adoption, RBI Pipeline analysis along with pipeline specific damage mechanism and consequence models on Criticality RBI Pipeline Segment will reach end of life and will be no longer available with the Q3 2025 release.
  • Published Inspections: The Published field will be removed from datasheets of Inspection families and related records and will no longer be automatically populated by APM from the Q1 2025 release.
  • Thickness Monitoring Dataloggers: The existing TM Datalogger GE DMS2 and Olympus (Panametrics) 37DL Plus Ultrasonic Thickness Gage will reach end of life and will be no longer available with the Q2 2025 release. We recommend all customers to use the rest of the existing dataloggers, i.e., GE DMS Go, GE DMS Go+, Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage, and Olympus Epoch 650.