Failure Elimination Workflow
Failure Elimination Workflow Overview
Failure Elimination Workflow (FEW) process is a step-by-step methodology that includes the following steps:
S.No | Step Name | Description |
---|---|---|
1 | Identify bad actors and trigger a Root Cause Analysis (RCA). | Identify the bad actors and then initiate an RCA to eliminate the root cause. |
2 | Assign an owner. | Assign an owner to the RCA who will work on the RCA. If, however, you want to hold on the RCA up to a certain date, you can de-escalate it. |
3 | Perform RCA. | Perform the RCA by identifying corrective and preventive actions (CAPA), their execution and evaluation of the effectiveness in eliminating the cause. You can use the existing RCA templates to create a Logic Tree. |
4 | Execute actions. | Implement the actions identified in the Recommendations to avoid future occurrence of the failure. |
5 | Evaluate actions. | After you implement the Recommendations, track the RCA using a Tracking Item, which allows you to define the threshold cost and count. You can also use the quarterly CM count and cost trends to understand the impact of the actions. If the actual cost and count for tracked assets exceed the threshold values, an email is sent to the RCA Owner, stating that the failure criteria is breached. |
6 | Mark the RCA complete. | If the RCA does not breach for a year, an email is sent to the RCA Owner. Using your discretion, you can continue to monitor the RCA or mark the RCA complete, and then mark the FE Workflow status complete. Even after the FE Workflow is marked, complete you can reopen it until the RCA is marked complete. |
Access the Failure Elimination Dashboard Page
Procedure
Step 1: Identify Bad Actors and Trigger RCA
About This Task
Procedure
What To Do Next
Step 2: Assign Owner
Before You Begin
About This Task
Procedure
- Access the Failure Elimination Dashboard page.
- In the FAILURE ELIMINATION WORKFLOW STEPS section, select Step 2: Assign RCA Owner.
- If you want to assign an RCA owner:
- If you want to de-escalate an RCA:
What To Do Next
Step 3: Perform RCA
Before You Begin
About This Task
Procedure
What To Do Next
Step 4: Execute Actions
Before You Begin
About This Task
Procedure
What To Do Next
Step 5: Evaluate Actions
Before You Begin
About This Task
If the actual cost and count for tracked assets exceed the threshold values, an email is sent to the RCA Owner, stating that the failure criteria is breached.