APM Client

Hardware Requirements

The following hardware requirements outline the minimum hardware required for any machine or mobile device that will access the APM system. These requirements account for the APM software only. Additional hardware may be required on clients where other components are installed. These requirements may not be sufficient, depending upon how your system is configured.

Desktops and Laptops

Minimum RequirementsRecommended Requirements for Optimal User Experience
Two Processor Cores, 2 GHzSix Processor Cores, 2.6 GHz (for example, Intel Core i7 9750 H- High performance CPU
4 GB RAM (16 GB RAM recommended)32 GB RAM
8 GB of available hard drive space512 GB Solid State Drive
13" screenGraphics Card with 4GB of RAM (for example, Nvidia Quadro series)
1024 X 768 screen resolution1920 X 1080 screen resolution

Mobile Devices

You can use APM on mobile devices either in the GE Digital APM mobile application or in the web browser on the device. The following information is generic and pertains to using the application on mobile devices in either of these scenarios. For specific information regarding the mobile application, see the GE Digital APM Mobile Application portion of the Getting Started section of this documentation.

Support for mobile devices is provided in two resolution view modes: full or limited. Full-resolution view mode supports access to the entire APM system. Limited-resolution view mode supports limited access to overview pages and data collection. Resolution view mode is determined by the type of device that is used to access APM, and is not a selectable option.

Note: Interaction with diagramming and design canvases is not available on touch-screen devices. If needed, use a mouse peripheral to utilize this functionality.
Minimum RequirementsDevices Tested

Minimum requirements for full-resolution view mode:

  • Two Processor Cores, 2 GHz
  • 2 GB RAM
  • 8 GB of available hard drive space
  • 7" screen
  • 1920 X 1200 screen resolution

Devices used in the APM testing environment:

  • Apple iPad 4th Generation
  • Apple iPad Air
  • Apple iPad Air 2
  • Apple iPad Mini 2
  • Apple iPad Mini 3
  • Microsoft Surface Pro 3

Minimum requirements for limited-resolution view mode:

  • Two Processor Cores, 1 GHz
  • 1 GB RAM
  • 8 GB of available hard drive space
  • 4" screen
  • 1024 X 600 screen resolution

Devices used in the APM testing environment:

  • Samsung Galaxy Tab 4 (7")
  • Samsung Galaxy Tab 4 (10")

Small Screen Devices

Note: You can access only the Rounds Data Collection module in portrait mode on small screen devices.
Minimum RequirementsDevices Tested

Minimum requirements:

  • Four Processor Cores, 1.3 GHz
  • 1 GB RAM
  • 8 GB of available hard drive space
  • Minimum screen resolution of 320 pixels wide in portrait mode (4" or larger physical screen size recommended)

Devices used in the APM testing environment:

  • Lenovo A1000 (480 X 800 screen resolution)

Software Requirements

The following software components are required on any machine or device that will access the APM system using a browser. If the software meets the following requirements, you can access APM using any operating system.

One of the following browsers is required for desktops, laptops, and mobile devices:

BrowserNotes
Latest version of Google Chrome

New versions of Google Chrome are released every 4 weeks. Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, we recommend that you use the latest Google Chrome version available.

Microsoft Edge

New versions of Microsoft Edge are released every 4 weeks. Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, we recommend that you use the latest Microsoft Edge version available.