SQL Server Report Server
Hardware Requirements
The following hardware requirements outline the minimum hardware required for any machine that will serve as the SQL Server Report Server. These requirements account for the APM software only. Additional hardware may be required on a SQL Server Report Server machine where other components are installed. These requirements may not be sufficient, depending upon how your system is configured.
Component | Requirement |
---|---|
Core | Two Processor Cores, 2+ GHz |
RAM | 8 GB RAM |
Hard Drive | 25 GB of available hard drive space |
If you are using a virtual machine (VM) to host your SQL Server Report Server, we recommend that:
- You increase the physical server CPU and hard drive space requirements by 20% to ensure that the application will perform equivalently in a virtualized environment.
- You double the physical server memory requirements.
- Each VM have its own dedicated processor cores and memory allocation to ensure appropriate performance.
APM supports Hyper-V and VMWare platforms.
These requirements may not be sufficient, depending on how your system is configured. Parameters that affect the hardware requirements include the number of users, modules purchased, database size, and other factors that can vary from one customer to another. For help refining your specific system requirements, consult a member of the APM Professional Services department.
Software Requirements
The following software components are required on any machine that will serve as the SQL Server Report Server.
Software Name and Version | Where You Can Obtain It | Required? | Behavior of APM Server Installer |
---|---|---|---|
Any of the following versions of SQL Server Reporting Services:
|
Microsoft |
Yes |
If it is not available, the installation fails. |