Schedules
About Rounds Pro Schedule
Rounds Pro Schedules are schedule objects that are maintained in the Rounds Pro Schedule Family. These schedules once created can be linked to Measurement Steps.
Advantages of using a schedule:
- You can organize your schedules and later associate them with Measurement Steps.
- You can use the same schedule in multiple steps. All these steps will then follow the same schedule. You can thus track all these steps easily.
- If you update a schedule, the changes are applied to all the steps that use the schedule.
Route Instance Examples Based on a Schedule
This topic provides information on how Route Instances are created with few examples of scheduling.
S.No | Route Master Schedule Status | Step Schedules (This example route has 5 steps) | Expected Result | ||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1 | Defined for everyday for 8 AM | Not Defined for any of the five steps. | A Route Instance is created every day at 8AM with all the five steps. | ||||||||||
2 | Defined once every 12 hours starting at 6 AM Note: Steps are usually scheduled at lower frequency than that for Route Master.
|
|
| ||||||||||
3 | Not Defined | Defined for everyday at 8 AM for all the steps. | This is a Invalid Scenario. |
Access a Rounds Pro Schedule
Procedure
Create a Rounds Pro Schedule
About This Task
You can create a schedule to use it in Measurement steps.