Data Loader
About the Geographic Information System (GIS) Data Loader
The GIS Data Loader allows geospatial data associated with existing APM entities to be imported into the GIS data model, so that information about the entities can be displayed in the Maps module in APM. You can load geospatial data using the provided Excel workbook.
About the GIS Data Loader Requirements
To use the GIS Data Loader, you must have existing entity records, for example, the Functional Locations or Equipment, that you want to associate with the geospatial data. To use the geospatial data in the Maps module, your organization must have completed the GIS Configuration steps.
Mapping
The GIS Data Loader inserts geospatial data in the MI_ENTY_GEO_DATA table and associates it with existing entities in APM. Entities are identified by mapping from specified cells in the Excel workbook to the ENTITY_KEY field. The data loader evaluates the data provided in the Excel workbook in the following order:
- ENTITY_KEY + FAMILY_ID
- ENTY_ID + FAMILY_ID
- FAMILY_ID + ID_FIELD + ID
About the GIS Data Loader Data Model
The following data model illustrates the records that the Data Loader supports.
GIS Data Loader Data Model
About the GIS Data Loader General Loading Strategy
The imported data must load in a specific sequence to successfully populate fields, create records, and link data to the predecessor and successor records.
Best Practices
When importing data using the GIS Data Loader, you must use the following Best Practices:
- To identify an existing record to associate with the geospatial information, use one of the following options:
- Specify the ENTITY_KEY and FAMILY_ID values.
- Specify the ENTITY_ID and FAMILY_ID values. If ENTITY_KEY is not provided, the data loader will search for the ENTITY_KEY matching the ENTITY_ID.
- Specify the FAMILY_ID, ID_FIELD, and ID values. If ENTITY_KEY and ENTITY_ID are not provided, the data loader will search for an ENTITY_KEY matching the specified values.
- If there is no existing record for the referenced Entity Key in the MI_ENTY_GEO_DATA table, and you provide valid geospatial data, a new record will be created in the MI_ENTY_GEO_DATA table.
- If there is an existing record for the referenced Entity Key in the MI_ENTY_GEO_DATA table, and you provide new valid geospatial data, the existing record in the MI_ENTY_GEO_DATA table will be updated.
- If there is an existing record for the referenced Entity Key in the MI_ENTY_GEO_DATA table, and you provide no geospatial data (i.e. the cell is empty), the record will be deleted from the MI_ENTY_GEO_DATA table.
- If the identifying values (i.e. either ENTY_ID + FAMILY_ID or FAMILY_ID + ID_FIELD + ID) provided in the worksheet match more than one entity record, the record in the MI_ENTY_GEO_DATA table will be associated with the first matching entity record that is found. If this occurs, a warning will be added to the import log.
- Geospatial data in the GEOD_DATA column should conform to the geometry spatial data type.Note: Valid geospatial data format is dependent on your APM database type. Points must specify Longitude first, then Latitude, in degrees. For example, the geospatial data for a point in Roanoke, Virginia, USA is defined as. POINT (-79.9372289704512 37.2698054035023) in SQL Server 2016.
Load Sequence
When importing data using the data loader workbook, you must use the following workflow:
- Download the data loader workbook provided by GE Vernova.
- Identify the data requirements for exporting the data into the data loader workbook.
- Extract data from APM and your GIS applications to populate the data loader workbook.
- Provide batch numbers in the first column of the worksheet in the data loader workbook.
- Import data into APM.
- Monitor the status of the data load, and verify the results in the log.
- Conduct tests in APM to ensure that the imported data loaded accurately.
For each row in the data loader workbook, the GIS Data Loader will insert, update, or delete a row in the geospatial data table in the APM system.
About the GIS Data Loader Workbook Layout and Use
In order to import data using the GIS Data Loader, APM provides an Excel workbook, Geographic Information System (GIS).xlsx, which supports the Maps tool in APM. This workbook must be used to perform the data load.
The following table lists the worksheets that are included in the GIS Data Loader workbook.
Worksheet | Description |
---|---|
GIS | The only worksheet used by the GIS Data Loader. It is used to load geospatial data for existing entities. |
The following table lists the fields in the workbook:
GIS Worksheet
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Batch ID | BATCH_ID | Character (50) | You must specify a Batch ID for each row in the worksheet. |
Entity Key | ENTITY_KEY | Numeric | You can use this column to specify the Entity Key field of the APM entity that you want to associate with the GIS data. |
Entity ID | ENTITY_ID | Character (255) | You can use this column to specify the Entity ID of the APM entity that you want to associate with the GIS data. |
Family ID | FAMILY_ID | Character (50) | You must specify the Family ID of the APM entity that you want to associate with the GIS data. |
Family ID Field | ID_FIELD | Character (50) | You can use this column to specify the Field ID of the field which will be used to identify the APM entity record that you want to associate with the GIS data. |
ID | ID | Character (255) | You can use this column to specify the identifying value in the Family ID Field of APM entity record that you want to associate with the GIS data. |
Geometry | GEOD_DATA | Character (4000) | You can use this column to specify the GIS data to be associated with the APM entity. If this column contains a null value, any existing GIS data associated with the APM entity will be deleted. |
About the GIS Data Loader Load Verification
About This Task
- Review the details of the import job. These details will indicate if any errors or warnings occurred during the data load. The log helps you identify any records that are not loaded.
- Run a query to view the geospatial data that was uploaded. You can use the baseline Map Query that is stored in the \\Public\Meridium\Modules\Core\Queries\Map Queries\ folder, as a reference.