Admin
Access the Deferral Configuration Page
Procedure
In the Applications menu, navigate to ADMIN > Application Settings > Deferral Configuration.
The Deferral Configuration page appears, displaying the Deferral Configuration workspace. You can view the configurations for each family that participate in the Has Deferral relationship family in the left navigation, and modify any necessary fields.
In the baseline APM database, Deferral Configuration is provided for the following families:
- Inspection Task
Note: The baseline configuration is provided for the above listed families, however, the Deferral workflow is not enabled by default. To enable, select the Enable Deferral option for the given family to enable the workflow.
Create or Modify a Deferral Configuration Record
When you view the Deferral Configuration page, if there are families that participate in the Has Deferral relationship, but are not included as part of the APM baseline database configuration, you can create the Deferral Configuration for that family. In addition, you can also modify settings of existing configuration records if desired.
Before You Begin
- Ensure that you have identified fields from the selected family, which will represent the original planned date and the updated deferred date.
Procedure
Define Deferral Limits By Site
About This Task
- Site-specific limit: Limits that apply to specific sites.
- Global limit: A top-level limit that applies to all records where the site of those records does not exist in any other Deferral Limit for the current Deferral Configuration.
- Global limit: 3
- Site-specific limit:
- Site B: 2
- Site C: 2
When approving deferrals for a record that belongs to Site A, you cannot approve more than 3 consecutive deferrals. If you are approving deferrals for a record in either Site B or Site C, you cannot approve more than 2 consecutive deferrals.