Static Data Adapter

About the Static Data Adapter

Using the Static Data Adapter, you can extract master data from the SAP system into an intermediate repository so that code conversion to description can be managed in the integration layer.The data can pertain to currency codes, UOM codes, plant codes, and so on. It is recommended that you execute this interface daily to keep the code mappings updated.

Static Data Interface is a prerequisite for the technical characteristics. Static Data Interface extracts all the Equipment and Functional Location characteristics from SAP and processes into APM. You can then select the characteristics based your requirement. Accordingly, the Technical Characteristics Interface extracts only the selected Equipment and Functional Location characteristics.

About the ASI Static Data Adapter

The ASI Static Data Adapter is an extension to the Static Data Interface to extract data codes specific to the ASI workflow into APM. After this data is available in APM, you can use it in the workflow to create the ASI package.