SQL Server Report Server

Hardware Requirements

The following hardware requirements outline the minimum hardware required for any machine that will serve as the SQL Server Report Server. These requirements account for the APM software only. Additional hardware may be required on a SQL Server Report Server machine where other components are installed. These requirements may not be sufficient, depending upon how your system is configured.

ComponentRequirement
CoreTwo Processor Cores, 2+ GHz
RAM8 GB RAM
Hard Drive25 GB of available hard drive space

If you are using a virtual machine (VM) to host your SQL Server Report Server, we recommend that:

  • You increase the physical server CPU and hard drive space requirements by 20% to ensure that the application will perform equivalently in a virtualized environment.
  • You double the physical server memory requirements.
  • Each VM have its own dedicated processor cores and memory allocation to ensure appropriate performance.

APM supports Hyper-V and VMWare platforms.

These requirements may not be sufficient, depending on how your system is configured. Parameters that affect the hardware requirements include the number of users, modules purchased, database size, and other factors that can vary from one customer to another. For help refining your specific system requirements, consult a member of the APM Professional Services department.

Software Requirements

The following software components are required on any machine that will serve as the SQL Server Report Server.

Software Name and VersionWhere You Can Obtain ItRequired?Behavior of APM Server Installer
Any of the following versions of SQL Server Reporting Services:
  • 2019
  • 2017
  • 2016

Microsoft

Yes

If it is not available, the installation fails.