SQL Server Analysis Services
Hardware Requirements
The following hardware components are the basic hardware that are required for supporting SQL Server Analysis Services in APM Metrics and Scorecards module. These requirements are specified only for the APM software. Additional hardware may be required on a SQL Server Analysis Services machine where other components are installed. These requirements may not be sufficient and may change depending upon how your system is configured.
Component | Requirement |
---|---|
Core | Two Processor Cores, 2+ GHz |
RAM | 8 GB RAM |
Hard Drive | 25 GB of available hard drive space |
Software Requirements
One of the following software is required on any machine that will serve as the SQL Server Analysis Services server.
Software Name and Version | Where You Can Obtain It |
---|---|
SQL Server Analysis Services 2014 (Multi-Dimensional mode only) | Microsoft |
SQL Server Analysis Services 2016 (Multi-Dimensional mode only) |