Instrumented Functions
About Instrumented Function
An instrumented function is a specific need of a safety instrumented system to monitor the conditions of a process. For each instrumented function defined for a safety instrumented system, at least one protective instrument loop (PIL) will exist to satisfy that need.
When you create an Instrumented Function, it will be linked automatically to the current SIL Analysis. When you create the Instrumented Function, in addition to details about the instrumented function, you can specify the following records linked to the Instrumented Function:
- Logic Solver
- Equipment and Functional Location
- SIF Common Cause Failures
- Hazardous events that may occur if the safe state associated with the current instrumented function occurs at the same time as the safe state associated with a different instrumented function.
Access an Instrumented Function
Procedure
Create an Instrumented Function
About This Task
This topic describes how to create an Instrumented Function using a blank datasheet. You can also copy an Instrumented Function.
Procedure
What To Do Next
Copy an Instrumented Function
About This Task
You can create an Instrumented Function by copying the details from another Instrumented Function linked to a SIL Analysis.
- External Assessment
- LOPA Assessment
- PHA Internal Assessment
- Risk Matrix Internal Assessment
- Protective Instrument Loop
- SIF Common Cause Failure
- SIS Proof Test Template
Family | Fields |
---|---|
External Assessment | External Assessment ID |
Instrumented Function |
|
LOPA Assessment | LOPA Assessment ID |
PHA Internal Assessment | Assessment ID |
Risk Matrix Internal Assessment | Risk Assessment Internal ID |
Protective Instrument Loop |
|
Protective Instrument Loop Logic Solver |
|
Protective Instrument Loop Logic Solver Channel |
|
Protective Instrument Loop System (Sensor/Final Element System) |
|
Protective Instrument Loop Group (Sensor/Final Element Group) |
|
Protective Instrument Loop Sensor |
|
Protective Instrument Device (Sensor/Final Element) |
|
Protective Instrument Loop Final Element |
|
SIF Common Cause Failure | CCF ID |
SIS Proof Test Template |
|
SIS Proof Test Template Detail |
|
Functional Test Detail |
|
You can also create an Instrumented Function using a blank datasheet.
Procedure
Create a Recommendation
Procedure
Results
- The Recommendation that you have created is listed in the Recommended Actions pane for the Instrumented Function and the related SIL Analysis.
Copy a Recommendation
About This Task
You can copy a Recommendation and link to an Instrumented Function that is associated to one or more SIL Analysis records.
When you copy a Recommendation, the Equipment and Functional Location details from the copied Recommendation is replaced with the newly selected Instrumented Function details.
Procedure
Results
- The Recommendation that you have copied is listed in the Recommendations pane for the selected Instrumented Function.
Access the Health Summary Page of an Asset
This topic describes how to access the Health Summary page of the Asset that is being protected by an Instrumented Function.
Before You Begin
- Ensure that the Equipment ID or the Functional Location ID fields in the Instrumented Function datasheet are populated with the values that correspond to the Asset that is being protected by the Instrumented Function.