Administration

GAA Administration Workflow

This workflow describes the process for adding a GAA Company, GAA Plant, and GAA Unit.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a APM module, refer to the APM Product Workflows documentation.
Define CompanyDefine PlantDefine UnitGAA Event Management WorkflowUnitDefine Configuration

Define Configuration

Persona: Solution Administrator

Define the configuration to be used in a GAA unit for generating reports.

Define Company

Persona: Solution Administrator

Define the GAA Company to represent the functional location that you want to use in GAA.

Define Plant

Persona: Solution Administrator

Define the GAA Plant to represent the functional location that you want to use in GAA.

Define Unit

Persona: Solution Administrator

Define the GAA Unit to represent the functional location that you want to use in GAA. You can also define additional Unit Capacities and configure and associate Regulatory reports for a GAA Unit.

Unit

Persona: Solution Administrator

Defining GAA Unit provides GAA Unit record, Unit Capacity record, and GAA Report record.

GAA Event Management

Persona: Operator or Supervisor

Define an event when operating status or capability of a GAA Unit changes.

Go to the GAA Event Management workflow.