Manage Health Indicators
Asset Health Manager: Manage Health Indicators Workflow
This workflow describes the process for implementing checkpoints (i.e., new health indicator sources) and health indicators to implement risk mitigation Actions that have been defined in an Asset Strategy.
Asset Strategy Management
Persona: Analyst (Asset Strategy)
Asset Strategy Management defines the health monitoring requirements for an asset, or asset class, based on understanding the underlying failure modes and effects, in combination with the criticality of the asset. This process identifies candidate failure modes where health monitoring offers a significant reduction in risk. This workflow assumes that the Strategy has been approved, an Action has been created for each Risk where a health indicator is the identified mitigation, and the Actions are not yet implemented.
Go to the Asset Strategy Management Workflow.
Other Workflows
Persona: Varies
Health Indicator sources are records that are created in other workflows. Health Indicator sources include:
-
Rounds checkpoints, i.e., Measurement Locations and Lubrication Requirements. These represent recurring scheduled tasks typically performed by asset operators, maintenance and lubrication technicians.
Go to related workflows: Manage Rounds Routes and Asset Strategy Management.
-
Content Map, such as time series machine data collected from online sensors, which is stored in a process historian.
Go to related workflow: Integrate with M2M Data Source.
-
Key Performance Indicators (KPIs), i.e. calculated asset performance parameters such as availability, reliability, etc.
Go to related workflow: Manage KPIs.
-
Health indicator without source, i.e. health indicators calculated by Policies.
Go to related workflow: Design Policy.
Implement Action as Rounds
Persona: Analyst (Strategy)
If a new Checkpoint is needed, implement a risk mitigation Action by a Rounds activity (Checkpoint, i.e., Measurement Location or Lubrication Requirement).
Checkpoints can be created from a template or template groups directly within the Asset Strategy implementation workflow.
Implement Action as HI Source
Persona: Analyst (Strategy)
If a new Checkpoint is not needed, implement a risk mitigation Action using existing health indicator sources that are created by other APM workflows.
For example, you might:
- Create health indicators to monitor data from an external data source (e.g., Content Map).
- Use a policy by creating a Health Indicator or an automated decision making process.
- Implement a Checkpoint in Rounds Designer as a source for health indicators. Go to the Manage Rounds Routes workflow for details.
As part of implementing the Action, the health indicator source record is linked to the asset (i.e., equipment or functional location).
Link Health Indicator Source to Asset
Persona: Solution Administrator (Health)
Provided that the system is correctly configured, health indicators will be created automatically when health indicator source records are linked to an asset. Linking source records to assets may be done using Data Loaders, in Record Manager, or within other workflows such as the Manage Rounds Routes workflow.
Go to the Assess Asset Health workflow.
Health Indicator Created
Persona: Automated Process
Once a health indicator source record is linked to a relevant asset (i.e., equipment or functional location), Health Indicator records are created automatically and will be visible for the asset in Asset Health Manager.
Go to the Assess Asset Health workflow.
Persona: Manual Process
Health indicators are created by the User with a User Interface for a particular OT Source Tag and Asset through the OT AHI Connector.
The OT AHI Connector creates the Content Map record that relates the Health Indicator, OT Source Tag, and Asset. This relationship delivers value in readings, subscriptions, and limits. For more information see, Content Mapping.
Asset Strategy Management
Persona: Asset Strategy Analyst
Once the required Health Indicators have been created, the Asset Strategy Management workflow resumes. The Health Indicators can be selected to implement the previously unimplemented Actions.
Go to the Asset Strategy Management Workflow.
Manage Performance Recommendations
Persona: Solution Administrator (Health)
A recommendation created from the Assess Asset Health workflow may request a change to the configuration of a health indicator, such as its limit values.
Go to the Assess Asset Health workflow or the Manage Performance Recommendations workflow.
Manage HI Configuration
Persona: Solution Administrator (Health)
Configure the Health Indicator source records to define health indicator limit values.
Limit values are stored on the Health Indicator Source record (example, Measurement Location) for automatically created health indicators and on the health indicators for others (example, Content Maps).