Create Charts using Queries

Create Charts using a Baseline or Custom Query

Procedure

  1. Access the Advanced Visualization page.
  2. In the Advanced Visualization home page, select Visualize Data.
    The Advanced Visualization Designer page appears, displaying a designer canvas to create the chart.
  3. Select the Add Data button.
    The Select Data Source window appears, displaying the available data sources.
  4. Navigate to the folder containing the data source associated with the query, and then select the data source.
    The Dimensions and Variables associated with the data source appear in the Advanced Visualization Designer page.
  5. As needed, design the chart, and then save the chart.
    Note:
    • When designing a chart, we recommend that you use the fields in the ROWS section that appear when you expand the RESPONSE node and then expand the ROWS node.
    • For more information on how to create and publish charts, refer to the help documentation integrated with Advanced Visualization.
    The chart is created.