Create Charts using Data Sources
Create Charts using Data Sources
About This Task
This topic describes how to create charts or dashboards using data sources in Advanced Visualization.
Procedure
- Access the Advanced Visualization page.
- Select Visualize Data.The Advanced Visualization Designer page appears, displaying a designer canvas to create the chart.
- Select the Add Data button.The Select Data Source window appears, displaying the available data sources.
- Select the data source using which you want to create the chart.Note: You can access the baseline data sources and folders containing the baseline data sources by default. If you want to use a specific data source to create the chart, navigate to the data source in the corresponding folder. You can also change the view to access the data sources for a tenant.The Dimensions and Variables associated with the data source appear in the Advanced Visualization Designer page.
- As needed, design the chart, and then save the chart.Note: For more information on how to create and publish charts, refer to the help documentation integrated with Advanced Visualization.The chart is created.Note:
For more information on creating charts, refer to KBA 000039563.
For more information of training videos on how to create visualizations, refer to Getting Started With WebFOCUS 8207.
For detailed documentation on how to create visualization, refer to Visualizing Data in 8207.