Thickness Measurements
About Thickness Measurements
Thickness Measurements represent readings that are recorded at locations on an asset or one of its components. They are created and linked to TMLs.
Details
A Thickness Measurement is a value that quantifies the thickness of a given TML at a specific point in time.
Each TML will have various types of Thickness Measurements, including:
- Base Measurement : The first measurement taken for the TML.
- Near Measurement : The second-most-recently-recorded measurement for the TML.
- Last Measurement : The most-recently-recorded measurement for the TML.
Base, Near and Last Measurements are not recorded in the Thickness Measurements themselves. Instead, they are determined for the TML Corrosion Analysis by evaluating how many Thickness Measurements exist, and when the Thickness Measurements were created. After you create a new TML, you will want to record the base measurement, which represents the first recorded reading for that TML. Additional Thickness Measurements will be created later, as measurement readings are taken throughout the life of the asset.
About Nominal and Actual Measurements
Each Thickness Measurement can be classified as either a nominal measurement or an actual measurement.
- A nominal measurement represents a reading that is not taken physically but is recorded from some other source, such as a design specification.
- An actual measurement represents a reading that is taken manually at the physical thickness measurement location on the equipment.
Details
Actual measurements are typically more accurate and result in calculations that are more representative of the actual asset. Nominal measurements may not be as accurate, but provide an efficient mechanism for recording initial measurement data.
Any nominal measurement value can be used in the creation of a nominal measurement. Nominal measurements are used only for the base measurement (i.e., the first measurement).
- Measurement data will be populated automatically for the initial Thickness Measurement linked to TMLs configured for nominal base measurements.
- Measurement data must be entered manually for Thickness Measurements that are linked to TMLs that are not configured for nominal base measurements.
Thickness Monitoring will use all active thickness measurements for performing TML Corrosion Analysis calculations. Nominal measurements will become inactive measurement automatically after two subsequent actual measurements have been recorded. In other words, if the Measurement Taken Date of any two actual measurements is after the Measurement Taken Date of a nominal measurement, the nominal measurement will become an inactive measurement.
About Skipped Measurements
GE Digital APM Thickness Monitoring provides the option to skip measurements. This applies when you want to satisfy inspection requirements, but do not want to take an actual measurement at the TML. When you skip a measurement, instead of creating a Thickness Measurement for a TML, you will create a Measurement Not Taken (MNT) record to store the inspection data.
Details
Some reasons that you may want to skip measurements include:
- The physical location of certain TMLs may be difficult to reach or may require a shutdown in order to take a measurement.
- Your organization may have a strategy that calculates based on a certain percentage of TML measurements for an asset.
- Resource limitations may make it difficult or impossible to take measurements at all TMLs on an asset or its components.
In order to skip measurements in Thickness Monitoring, the Allow Measurements to be Skipped check box must be selected on the TM Admin Preferences page. Then you will need to create MNT records to represent any measurement that was skipped. After you have enabled this option and created MNT records, Corrosion Analyses containing skipped measurements will be updated to take those MNT records into account.
Skipping Measurements Consecutively
If you enable the option to skip measurements in TM, you will also have the option to enable a feature that allows you to skip measurements consecutively. When you do this, you will be able to create successive MNT records.
Example: Skipping Measurements Consecutively
Suppose that the TML TML01 is difficult to reach. As a result, your organizational policy dictates that while readings for all other TMLs on the associated piece of equipment must be taken every six months, a reading for TML01 must be taken only once per year, as illustrated in the following table.
TML | Scheduled Readings |
---|---|
TML01 |
June 1, 2014 June 1, 2015 |
TML02 |
June 1, 2014 December 1, 2014 June 1, 2015 December 1, 2015 |
TML03 |
June 1, 2014 December 1, 2014 June 1, 2015 December 1, 2015 |
Suppose that you create an MNT record when a reading is skipped for TML01 on December 1, 2014. Next, suppose that, due to budget constraints at your facility, the scaffolding necessary to gain access to TML01 is unable to be built on June 1, 2015 (the date on which an actual thickness measurement reading is scheduled to be taken for this TML). In this case, you may want to create another MNT record for TML01, assuming that an actual measurement will be taken when possible.
Interpreting Calculations in Corrosion Analyses that Include Skipped Measurements
When active Thickness Measurements and MNT records exist in a Corrosion Analysis, all calculations, with the exception of Interval Next Inspection Date, are calculated as if MNT records are not included in your Corrosion Analysis.
Consider the calculation for Short Term Corrosion Rate. Short Term Corrosion Rate is calculated using the Short Term Loss and Short Term Interval, where:
Short Term Corrosion Rate = Short Term Loss / Short Term Interval
...where:
Short Term Loss = Near Measurement Value - Last Measurement Value
...and:
Short Term Interval = Last Measurement Date - Near Measurement Date
Example: Corrosion Analyses that Include Skipped Measurements
Consider the following measurements.
ReadingDateMeasurement (inches)
Reading | Date | Measurement (Inches) |
---|---|---|
Base | 1/1/1985 | .2 |
N/A | 1/1/1987 | <Measurement Not Taken> |
Near | 1/1/1990 | .195 |
N/A | 1/1/1993 | <Measurement Not Taken> |
Last | 1/1/1995 | .19 |
N/A | 1/1/2000 | <Measurement Not Taken> |
Short Term Loss = .195 - .19
Short Term Loss = .005
Short Term Interval = 1/1/1995 - 1/1/1990
Short Term Interval = 5 years
Short Term Corrosion Rate = .005 / 5
Short Term Corrosion Rate = .001
The Short Term Loss was not calculated using a Last Measurement Value of 1/1/2000, the date in the MNT record that is associated with the most recent inspection of this TML. There is no value associated with this date (or the date in ANY MNT record) and therefore, these records are ignored in all calculations with the exception of Interval Next Inspection Date.
Interval Next Inspection Date
When MNT records are included in a Corrosion Analysis, Interval Next Inspection Date is calculated using the following equation:
Interval Next Inspection Date = Last Measurement Date + Default Inspection Interval
Where Last Measurement Date is the most recent value in the Measurement Taken Date field of both the active Thickness Measurement and active MNT records linked to a given TM
Example: Interval Next Inspection Date
Consider a Default Inspection Interval of 60 months (i.e., 5 years) and a TML that is linked to records with the following Measurement Taken Dates:
Record | Measurement Taken Date |
---|---|
Thickness Measurement | 1/1/2004 |
Measurement Not Taken | 1/1/2005 |
Thickness Measurement | 1/1/2006 |
Measurement Not Taken | 1/1/2007 |
In this case, the Interval Next Inspection Date would be calculated as:
Interval Next Inspection Date = 1/1/2007 + 60 months
Interval Next Inspection Date = 1/1/2012
Skipped Measurements and TML Corrosion Analysis Fields
When the most recent date is from an MNT record, and when the Corrosion Rate of a TML is less than the Controlling Corrosion Rate of the asset, the following fields in the TML Corrosion Analysis are populated with data based on the Controlling Corrosion Rate:
- Asset Average Corrosion Rate
- Asset Average Corrosion Rate Remaining Life
- Asset Average Corrosion Rate Retirement Date
- Asset Average Corrosion Rate Next Inspection Date
This differs from when the fields are populated in a Corrosion Analysis that does not include skipped measurements.
Example: Skipped Measurements in TML Corrosion Analysis Fields
Consider an asset with:
- An Asset Corrosion Analysis with a Controlling Corrosion Rate of 2.9 Mils/year.
- A TML Corrosion Analysis for a TML linked to the asset, with a Corrosion Rate of 2.2 Mils/year. The most recent measurement date is from an MNT record.
In this case, the Asset Average Corrosion Rate would be set to 2.9 Mils/year.
This Asset Average Corrosion Rate value could be the result of any method that is specified to determine the asset controlling corrosion rate (Maximum, Average, or Formula). This differs from a Corrosion Analysis that does not include skipped measurements. When a Corrosion Analysis does not include skipped measurements, the Asset Average Corrosion Rate field is populated only when certain settings are specified, and this value can be the result only of an Average or Formula method.
Asset Average Corrosion Rate is an input to some of the calculations that are used to populate the Asset Average Corrosion Rate Remaining Life, Retirement Date, and Next Inspection Date fields. These calculations are performed using the same formulas that are used when a Corrosion Analysis does not include skipped measurements. The results of the same calculations in a Corrosion Analysis that includes skipped measurements versus a Corrosion Analysis that does not include skipped measurements, however, may differ because of the values that will be used to populate the Asset Average Corrosion Rate field in each of these Corrosion Analyses.
In every case, the value selected will be the most conservative (i.e., highest) corrosion rate, whether from the TML Corrosion Analysis Corrosion Rate field, or the Asset Corrosion Analysis Controlling Corrosion Rate field.
How Measurement Values Are Determined
The final value associated with a Thickness Measurement is stored in the Measurement Value field. Values are not, however, entered directly into the Measurement Value field itself. Instead, values are entered into the Readings field.
To determine the Measurement Value for a Thickness Measurement, one or more readings will be collected at a given TML. To account for the margin of error associated with user error, equipment malfunction, or environmental conditions, you may wish to collect multiple readings for each Thickness Measurement. The number of readings that you may take for a measurement will depend upon various factors, including your company's policies, the characteristics of the TML, and the method that you are using to collect the readings. The number of readings that you must take for each measurement is determined by the value specified in the Number of Readings field in the TML to which the Thickness Measurement is linked.
After you have determined how many readings you must take for a specific measurement and have collected those readings, you will add a Thickness Measurement and log the reading values in the Readings box. A calculation will be performed against the values in the Readings box, based on the settings that you have defined for measurement readings. Then, the Uncorrected Measurement field will be populated with the result of that calculation. Finally, the Measurement Value field will be populated with the value in the Uncorrected Measurement field. The Measurement Value field will then contain a value representing the final, corrected thickness measurement value.
About Measurement and Corrosion Rate Variance
This topic has been intentionally excluded from the GE Digital APM product documentation website. Contact GE Digital Support to get access to this topic.
About Measurement and Corrosion Rate Variance Validation
This topic has been intentionally excluded from the GE Digital APM product documentation website. Contact GE Digital Support to get access to this topic.
About Measurement Correction Based on Growth
Thickness Measurements can be automatically corrected if they contain a value that is greater than a previous measurement.
About This Task
A Thickness Measurement is a growth if the value in the Uncorrected Value field is greater than the value in the Measurement Value field of the preceding measurement. GE Digital APM can automatically detect this growth scenario and update the measurement to correct it. To enable this functionality, you must select the Correct Measurements Based on Growth check box in the TM Admin Preferences page on the Global Preferences workspace.
When a measurement is corrected based on growth, the following actions happen:
- The Measurement Value field of the measurement is updated with the value from the Measurement Value field of the preceding measurement. The value in the Uncorrected Measurement field is left as it is to be used later for future updates or comparisons.
- The Basis for Measurement Correction field is set to Growth to indicate that the value was changed and the reason for change.
Measurement correction occurs during the following scenarios:
- When a measurement is created against a Thickness Measurement Location. During this scenario, the measurement being created is evaluated and updated accordingly. Also, if the measurement was inserted between any existing measurements, the measurements following the newly created measurement are evaluated for growth and updated accordingly.
- When a measurement is updated, if the Check for Growth field is set to true prior to saving the record, the measurement is evaluated for growth and updated accordingly. Also, other measurements on the same related Thickness Measurement Location are evaluated and updated accordingly.
- A Thickness Measurement that is preceded by a Nominal Thickness Measurement will not have its value corrected for growth as it is considered the first actual measurement to be taken for that TML.
- When a Thickness Measurement is deleted, the set of remaining measurements are not corrected automatically for growth. If a correction for growth is required, it is recommended to set the Status Indicator field of the Thickness Measurement to Inactive and set the Check for Growth field to true to force a correction for growth.
Examples
Scenario 1: Inserting a measurement with growth at the end of a collection
Assume the following collection of measurements exists where the highlighted row is being added as a new measurement.
Measurement Taken Date | Uncorrected Value (Inches) | Measurement Value | Basis for Measurement Correction |
---|---|---|---|
January 1, 2010 | .75 | .75 | |
January 1, 2015 | .73 | .73 | |
January 1, 2020 | .735 | .73 | Growth |
In this scenario because the value being entered on January 1, 2020, contains a growth over the value on January 1, 2015, its Measurement Value field gets updated with the previous measurement value and the Basis for Measurement Correction is updated to Growth.
Scenario 2: Inserting a measurement in the middle of a collection which creates a growth scenario
Assume the following collection of measurement exist where the highlighted row is being inserted in between the existing measurements.
Measurement Taken Date | Uncorrected Value (Inches) | Measurement Value | Basis for Measurement Correction |
---|---|---|---|
January 1, 2005 | .75 | .75 | |
January 1, 2010 | .73 | .73 | |
January 1, 2015 | .72 | .72 |
Now assume a measurement with a value of .724 is created on January 1, 2008. The measurements will now look like:
Measurement Taken Date | Uncorrected Value (Inches) | Measurement Value | Basis for Measurement Correction |
---|---|---|---|
January 1, 2005 | .75 | .75 | |
January 1, 2008 | .724 | .724 | |
January 1, 2010 | .73 | .724 | Growth |
January 1, 2015 | .72 | .72 |
Scenario 3 – Updating a measurement
Assume the following collection of measurements exist where the measurements have already been corrected for growth
Measurement Taken Date | Status Indicator | Uncorrected Value (Inches) | Measurement Value | Basis for Measurement Correction |
---|---|---|---|---|
January 1, 2005 | Active | .75 | .75 | |
January 1, 2008 | Active | .724 | .724 | |
January 1, 2010 | Active | .73 | .724 | Growth |
January 1, 2015 | Active | .72 | .72 |
Now, assume that the measurement on January 1, 2008, was determined to be inaccurate and has its Status Indicator field set to Inactive, the Check for Growth field is to true, and saved. The set of measurements would look like the following:
Measurement Taken Date | Status Indicator | Uncorrected Value (Inches) | Measurement Value | Basis for Measurement Correction |
---|---|---|---|---|
January 1, 2005 | Active | .75 | .75 | |
January 1, 2008 | Inactive | .724 | .724 | |
January 1, 2010 | Active | .73 | .73 | |
January 1, 2015 | Active | .72 | .72 |
Because the measurement on January 1, 2008, was made inactive, the value from the measurement on January 1, 2010, of .73 is now being compared with the value from the measurement on January 1, 2005, which is no longer a growth. As a result, the Measurement Value field of the measurement on January 1, 2010, is reset to its Uncorrected Value and the value Growth is removed from the Basis for Measurement Correction field.
Access Thickness Measurements
About This Task
- TMLs
- Measurements
Procedure
- To access Thickness Measurements in the TMLs section, perform the following steps:
- To access Thickness Measurements in the Measurements section, perform the following steps:
Add a Thickness Measurement
Before You Begin
- If you are recording readings for multiple Thickness Measurements, you can use the Measurement Data Entry workspace. Additionally, you can use a datalogger to record Thickness Measurement readings.
Procedure
What To Do Next
Add a Nominal Measurement
Procedure
Results
Create Measurement Not Taken (MNT) Records
Before You Begin
Optionally, you can also select the Allow Consecutive Measurements to be Skipped check box to allow the recording of multiple consecutive MNTs for a single TML without the recording of an actual measurement.
Procedure
Modify a Thickness Measurement
Procedure
Use the Measurement Data Entry (MDE) Workspace
Procedure
Results
- For each reading that is saved, a Thickness Measurement is created and linked to the corresponding TML.
- You can now recalculate the corrosion analysis.