Thickness Monitoring Export
About Thickness Monitoring Export
When to Export
- You want to re-assess existing TM data based on triggers such as time, process variations, inspection, or thickness updates.
- You want to quickly modify existing TM data in bulk. After exporting the records into an Excel spreadsheet, make the changes as needed, and re-import the records using the Thickness Monitoring (TM) Data Loader.
What to Export
The list of assets that appears in the Thickness Monitoring Export workspace is based on the following catalog query: Public\Meridium\Modules\Thickness Monitoring\Queries\Export Select Asset Query. By default, this query returns the assets whose Asset Controlling Next Inspection Date field contains a value and fall within the selected level of Asset Hierarchy.
The Export Select Asset Query has the Asset parameter; the query returns the underlying assets of the selected value in the Asset Hierarchy. By default, the Asset parameter is set to the current asset context provided in the Thickness Monitoring Overview page.
Worksheet | Family |
---|---|
Assets | Equipment and Functional Location |
Asset_CAS | Corrosion Analysis Settings |
TML_Group | TML Group |
TML_Group_CAS | Corrosion Analysis Settings |
TML | Thickness Measurement Location |
TML_CAS | Corrosion Analysis Settings |
Measurements | Thickness Measurement |
Worksheet | Family |
---|---|
Assets | Equipment and Functional Location |
Asset_CAS | Corrosion Analysis Settings |
Piping_Component | TML Group |
Piping_Component_CAS | Corrosion Analysis Settings |
Piping_Band | TML Group |
Piping_Band_CAS | Corrosion Analysis Settings |
TML | Thickness Measurement Location |
TML_CAS | Corrosion Analysis Settings |
Measurements | Thickness Measurement |
Thickness Monitoring Export Data
The Thickness Monitoring Export allows you to review the TML and related data in bulk, and then import it to GE Digital APM. The data is exported in the same format used by the Thickness Monitoring (TM) Data Loader to enable importing and updating data.
Worksheet | Lookup Fields |
---|---|
Asset | Equipment ID, CMMS System, and Equipment Technical Number |
Asset_CAS | Component and Inspection Type in addition to the Asset lookup fields |
TML_Group | TML Group ID in addition to the Asset lookup fields |
TML_Group_CAS | Inspection Type in addition to the TML_Group lookup fields |
TML | TML ID in addition to the TML_Group lookup fields |
TML_CAS | Inspection Type in addition to the TML lookup fields |
Measurements | Same as the TML lookup fields |
Worksheet | Lookup Fields |
---|---|
Asset | Equipment ID, CMMS System, and Equipment Technical Number |
Asset_CAS | Component and Inspection Type in addition to the Asset lookup fields |
Piping_Component | Component ID in addition to the Asset lookup fields |
Piping_Component_CAS | Inspection Type in addition tot he Piping_Component lookup fields |
Piping_Band | Piping Band ID in addition to Piping_Component lookup fields |
Piping_Band_CAS | Inspection Type in addition to Poping_Band lookup fields |
TML | Position in addition to the Piping_Band lookup fields |
TML_CAS | Same as the TML lookup fields |
Measurements | Same as the TML lookup fields |
- System Fields: You cannot edit these fields. These fields are maintained by GE Digital APM.
- Output Fields: These fields are calculated. You cannot set these fields.
- For Piping_Component, the MI_PIP_COMP datasheet is used to retrieve the fields.
- For Piping_Band, the MI_PIP_BAND datasheet is used to retrieve the fields.