Policy Execution
About Policy Execution
- Automatic execution
- Scheduled execution
- Manual execution
- You can execute only the active instances associated with active Policies.
- The policy execution log can grow quickly and significantly impact the size of the GE Digital APM database. You can control how quickly the execution log grows by modifying the execution history settings for each policy.
Automatic Execution
When automatic execution is configured, individual Policy instances are executed when records belonging to the Policy instance are updated. Additionally:
- For records represented by a Measurement Location, OT Connect Tag, or Health Indicator node, Policy execution is also triggered by changes in related Reading records in the APM database. However, for Health Indicator nodes, if a reading with a timestamp earlier than the latest reading processed by the health indicator service is added or updated,the policy will not be triggered, because the Asset Health Indicator service does not update the health indicator record in this case.Note: When you configure a policy with a Health Indicator node for Automatic Execution, the Asset Health Indicator service must be running in order for new readings to trigger a policy execution.
- For process historian tags represented by an OT Connect Tag node, Policy execution is also triggered when new readings are added in the process historian. Note: When you configure a policy with an OT Connect Tag node for Automatic Execution, the OT Connect Adapter service must be running in order for new readings to trigger a policy execution.
Automatic execution works in conjunction with the selection in the Trigger check box that appears on the Properties window for all Input nodes except Query, Constant, and Point Value nodes. When the Trigger check box is:
- Selected: Changes in a record or related readings represented by the node will trigger Policy execution. The Trigger check box is selected by default.
- Cleared: Changes in a record or related readings represented by the node will not trigger Policy execution.
For example, you have a Policy that contains an Entity node that represents an Equipment record, but the Entity node does not influence any of the logic in the Policy model that determines if action is needed. Rather, other Entity nodes (for example, representing Measurement Location records that are linked to the Equipment record) influence the actual logic in the Policy model. In this case, you can exclude the associated Equipment record from triggering the Policy execution by clearing the Trigger check box for that node. By doing this, only the changes in the relevant records will trigger Policy execution.
When Should Automatic Execution Be Used?
Use automatic execution when the Policy is designed to monitor one or more values that change with time and when an action is needed in response to a specific change. Consider the following examples:
- The Policy monitors readings related to an OT Connect tag. When a reading value crosses a defined threshold, the Policy creates or closes a Policy event.
- The Policy monitors the status of a Health Indicator record. When the Health Indicator enters the Alert state, the Policy sends an email to the responsible user.
Scheduled Execution
When scheduled execution is configured, all active instances that are associated with a Policy are executed according to the schedule that you define.
When Should Scheduled Execution Be Used?
Use scheduled execution when the Policy is designed to evaluate data over a period or when automatic execution could produce misleading results.
Consider the following examples of Policies designed to evaluate data over a period:
- Using the Threshold Statistics node, the Policy analyzes threshold excursions during the previous month for values related to an OT Connect tag or Health Indicator.
- The Policy evaluates conformance to an asset strategy by comparing the actual count of readings added for a measurement location within the previous week to the expected count.
Consider the following example of a Policy monitoring values where automatic execution could produce misleading results:
The Policy evaluates combined information from a Rounds Route that includes multiple measurement locations for a single asset.Because mobile users can enter readings in any order and could change a previously entered reading value before finalizing the Route, using automatic execution in this scenario could trigger executions where one or more readings are from an earlier Route execution or are otherwise invalid.
Instead of using automatic execution, the Policy could be scheduled to run at a similar frequency to the Route. For example, if the Route is completed during the morning shift on weekdays, the Policy could be scheduled to execute after the end of the shift. The Policy checks whether new Readings have been added for all the required inputs before proceeding with the evaluation of the results.
Considerations for Scheduled Policies
You can take steps to prevent delays in Policy execution by considering the number of Policies you are scheduling and the number of instances associated with each.
When scheduling multiple Policies, you can configure the Policy for different schedules so that the executions are staggered throughout the day.
All active instances of a scheduled Policy are submitted for execution at the same time. Therefore, when scheduling a Policy with a large number of instances, you can stagger the executions by creating multiple copies of the Policy, each with a subset of the instances. You can then schedule each of the Policies to be executed at a different time. This approach may be especially advantageous when users are located in multiple time zones, as you could configure relevant Policy instances to be executed outside of normal business hours such that results are available in different locations as needed.
Manual Execution
If a Policy is active, you can manually execute the Policy irrespective of the configured execution settings. You can execute an active instance or all the active instances associated with the Policy. If you manually execute a Policy, the execution settings configured for the Policy are not changed and the Policy continues to be executed according to the configured settings.
When Should Manual Execution Be Used?
If you want the Policy to trigger the specified actions once without changing the existing execution settings that are configured for the Policy or configuring additional one-time scheduled execution settings, you can use the manual execution method.
- Sending an email
- Applying an Asset Strategy Template
For example, you designed a new Policy for an electric motor such that if the working temperature of a motor exceeds 800 K, an email notification will be triggered to the related engineer. You created two instances for the Policy and activated them without activating the Policy. Based on the requirement of the Policy, you configured it for automatic execution. Now, if you want to verify if the newly created Policy correctly triggers the required email notification, you must additionally configure the Policy for a one-time scheduled execution and activate the Policy. In this scenario, you can manually execute the Policy and verify if it triggers the correct action, instead of configuring additional one-time execution settings.
About Active Policies and Policy Instances
When a policy is active, the active instances that are associated with the policy will be executed according to the execution settings defined for the policy.
Consider a policy with two instances, where one instance is active and another instance is inactive.
- If the policy is active, the active instance will be executed according to the execution settings defined for the policy.
- If the policy is inactive, neither of the policy instances will be executed. However, the active instances associated with an inactive policy can be executed if the policy is manually executed and is not according to the pre-configured execution settings.
If a policy is active but does not contain an active instance, a warning message appears in the notification bar, indicating that there are no active instances to execute.
Configure Scheduled Execution
Before You Begin
- Run the validation process to confirm that the policy logic is working correctly.
- Verify that the correct time zone is specified for the policy.
About This Task
Procedure
Results
What To Do Next
Configure Automatic Execution
Before You Begin
- Run the validation process to confirm that the policy logic is working correctly.
About This Task
Procedure
Results
What To Do Next
Execute an Active Instance Manually
Before You Begin
- Run the validation process to confirm that the policy logic is working correctly.
About This Task
You can manually execute an active instance or all the active instances associated with a Policy. This topic describes how to execute a specific active instance associated with a Policy.
Procedure
Execute all Active Instances Manually
Before You Begin
- Run the validation process to confirm that the policy logic is working correctly.
About This Task
You can manually execute an active instance or all the active instances associated with a Policy. This topic describes how to execute all the active instances associated with a Policy at once.
Procedure
Activate or Deactivate a Policy
Before You Begin
- Run the validation process in order to confirm that the policy logic is working correctly.
- Configure the execution settings for the policy.
Procedure
Results
- If you activated the policy, the active policy instances that are associated with the policy will be executed according to the policy's execution settings.
- If you deactivated the policy, none of the policy instances that are associated with the policy will be executed.
What To Do Next
Configure Policy Execution History Log Setting
About This Task
You can configure the policy to determine when execution history log records will be created.
Procedure
Access Execution History
Procedure
Monitor Policy Execution
About This Task
When you execute a policy, a notification is sent to the policy trigger queue. A policy trigger service processes the requests and sends a message to the policy execution queue. A policy execution service processes this message and executes the policy. Depending on the load on the policy execution service, the start time of the policy execution varies.
The policy execution history contains the time that the notification was sent to the policy trigger queue, the execution start time, and the execution end time for each policy execution.
You can monitor the average and maximum wait times and review recent policy executions on the Policy Designer Overview page and the Recent Policy Executions dashboard.
Procedure
- To view policy execution details on the Policy Designer Overview page:
- Access the Policy Designer Overview page.
- Access the AVERAGE AND MAX WAIT TIMES IN QUEUE FOR 15 MIN INTERVALS IN LAST 4 HOURS Graph.
- To view policy execution details on the Recent Policy Executions dashboard:
About Execution History Logs
Execution history logs are stored in a non-family table, MI_POLICY_EXEC_LOG, in the APM database. You can access these records using a query by typing the code directly into the SQL tab of the query designer. This table contains logs for both Policy Designer and Family Policy executions.
Execution History Log Fields
The following table describes the fields in the MI_POLICY_EXEC_LOG table.
Field ID | Data Type | Description |
---|---|---|
MI_POLICY_EXEC_LOG.PLOG_KEY | String | Unique key of the execution history log record |
MI_POLICY_EXEC_LOG.PLOG_KEY | String | Unique key of the execution history log record. |
MI_POLICY_EXEC_LOG.POLICY_KEY | String | Entity Key of the related policy. Empty for family policy execution records. |
MI_POLICY_EXEC_LOG.INST_KEY | String | Entity Key of the related policy instance. Empty for family policy execution records. |
MI_POLICY_EXEC_LOG.PLOG_START_TM | Date and Time | Start of execution. |
MI_POLICY_EXEC_LOG.PLOG_TRIG_TM | Date and Time | Start of processing by the policy trigger service. Empty for family policy execution records. |
MI_POLICY_EXEC_LOG.PLOG_END_TM | Date and Time | End of execution. |
MI_POLICY_EXEC_LOG.PLOG_ACTION_TAKEN_FLG | Boolean | True if an action node was executed. |
MI_POLICY_EXEC_LOG.PLOG_ERRORS_FLG | Boolean | True if an error occurred. |
MI_POLICY_EXEC_LOG.PLOG_WARNINGS_FLG | Boolean | True if a warning occurred. |
MI_POLICY_EXEC_LOG.PLOG_SUMMARY_MEM | Text | Summary of the policy execution results. Displayed in the Execution History tab in Policy Designer or Family Policy. |
MI_POLICY_EXEC_LOG.PLOG_REV_NBR | Integer | Revision number of the policy model when the policy was executed. If this value is equal to the current policy model revision, the execution history details can be displayed in the design canvas. |
MI_POLICY_EXEC_LOG.PLOG_DATA_TX | Text | Detailed policy execution results in JSON format. |
MI_POLICY_EXEC_LOG.FAMPOLICY_KEY | String | Entity key of the related family policy. Empty for Policy Designer execution records. |
MI_POLICY_EXEC_LOG.TRIGGERED_BY_CHR | String | Information about how the policy execution was triggered. |
Example Execution History Log Query
The query shown below retrieves policy designer execution history log records where an Add Value to Health Indicator node was executed, with execution start time between March 1 and March 31, 2023:
SELECT [MI_POLICY].[MI_POLICY_ID_C] "Policy Name"
, MI_POLICY_EXEC_LOG.POLICY_KEY "Policy Key"
, MI_POLICY_EXEC_LOG.PLOG_START_TM "Start Time"
, MI_POLICY_EXEC_LOG.PLOG_SUMMARY_MEM "Summary"
FROM MI_POLICY_EXEC_LOG
JOIN [MI_POLICY] ON MI_POLICY_EXEC_LOG.POLICY_KEY = [MI_POLICY].ENTY_KEY
WHERE (MI_POLICY_EXEC_LOG.PLOG_START_TM >= '2023-03-01' AND MI_POLICY_EXEC_LOG.PLOG_START_TM < '2020-04-01' AND MI_POLICY_EXEC_LOG.PLOG_SUMMARY_MEM LIKE '%Add Value to HI%')