Admin

Access the Policy Admin Page

About This Task

You can use the Policy Admin page to configure the retention settings for the execution history records of policies created using Policy Designer.
Important: You can access the Policy Admin page only if you are a member of the MI Policy Administrator security group.

Procedure

In the Applications menu, navigate to ADMIN > Application Settings > Policy Designer.
The Policy Admin page appears, displaying the Execution History Settings workspace.

Configure Execution History Retention Settings

About This Task

The Policy execution log can grow quickly and significantly impact the size of the APM database. You can control the size of the execution log by minimizing the time that the execution history is retained in the APM system and also by selecting an appropriate execution history setting for each policy.

By default, the Policy Execution History records are never deleted. This topic describes how to set a retention period and the time interval of an automated job that deletes these records after the retention period is over.

The following conditions apply when you set the retention period:
  • These settings are applicable to all types of Policies and Policy Execution History records: Errors, Warnings (Action Taken), Warnings (No Action Taken), Success (Action Taken), and Success (No Action Taken).
  • The most recent execution history of each instance associated with a Policy is retained even if it exceeds the specified retention duration.
  • Depending on the number of old Policy Execution History records that exist when the retention settings are configured, it may take multiple iterations of the automated job to delete all the old execution history records.

Procedure

  1. Access the Policy Admin page.
  2. For each execution result type for which you want to change the retention period, perform the following steps:
    1. In the Execution History Settings workspace, in the Retention Period section, select Duration.
      The Duration and Every fields appear.
    2. In the Duration box, enter the duration in months for which you want to retain the records.
  3. In the Every box, enter the time interval at which the automated job must run to delete old Policy Execution History records.
    By default, the time interval that you enter is defined in hours. However, you can select the required unit from the drop-down list box to specify the interval in other units of time.
  4. Select Save.
    The execution history settings are configured.

About API Node Credential Records

API Node Credential records are used to store the user names, authentication types, and display names for user accounts that will be used by the system when executing API nodes in Policy Designer.

Note: Authentication type is set to APM by default.

When you create or update an API Node Credential, you must enter the user’s current password. The password not stored; it is only used to authorize permission to use that user account as an API Node Credential. If the API user’s password is changed you do not need to re-enter it through the Policy Admin page.

The user accounts that you specify in API Node Credential records must have the appropriate permissions to execute the APIs that you want to use in the API node. For information on supported APIs, see the API Node documentation.

Each API Node Credential must contain a unique value for display name. This is the name that will be displayed to Policy Designer users and should be descriptive to enable them to identify the correct user for the API they want to use. Policy Designer users will only see the display name and authentication type; they will not have access to the username or password.

You can set up any number of API Node Credentials as required. For example, you might want to set up different API Node Credentials for access to different APIs.

Add API Node Credential Records

Procedure

  1. Access the Policy Admin Page
  2. Select the API Node Credentials section.
  3. Select
    The API Node User Details window appears.
  4. Enter the Display Name, Username and Password.
  5. Select Save.

Results

The credential is saved and displayed in the list of available credentials in the API Node the next time you open a new Policy Designer page.

Update API Node Credential Records

Procedure

  1. Access the Policy Admin Page
  2. Select the API Node Credentials section.
  3. In the grid, select the credential that you want to edit and then select
    The API Node User Details window appears.
  4. Update the credential information as required.
  5. Re-enter the Password.
  6. Select Save.

Results

The credential is updated.

Delete API Node Credential Records

Procedure

  1. Access the Policy Admin Page
  2. Select the API Node Credentials section.
  3. In the grid, select the credential that you want to delete and then select
    A Confirmation Dialog Box appears.
  4. Select OK.

Results

The credential is deleted. Any policies containing API nodes configured to use the credential will no longer execute successfully.