SRS Projects
About SRS Project
Creation of an SRS Project allows the user to select one or many of the SRS templates. Once the user has made the selection of templates, a copy of the collection of templates will be made.
The user can link the SRS Project to zero or many of the following elements:
- SIL Analysis
- Logic Solver
- Instrumented Function
- Protective Loop
The linkage takes place in the context of a linkable item (for example, instrumented function) where the user can search and select an approved SRS Project.
Access an SRS Project
Procedure
Create an SRS Project
Before You Begin
Procedure
Results
- The SRS Project that you created appears in the SRS section of the SIS Management Overview page.
What To Do Next
Access the List of Linked Records in an SRS Project
Procedure
Change the State of an SRS Project
Procedure
Results
- Based on the state of the SRS Project, the datasheet is either enabled or disabled for modification:
- If the state of the SRS Project is changed to Pending Review, the datasheet is disabled.
- If the state of the SRS Project is changed to In Progress, the datasheet is enabled.
- If the state of the SRS Project is changed to Pending Review, the datasheet is disabled.
- If the state of the SRS Project is changed to Approved, the datasheet is disabled. At this stage, the revision number is incremented.
Access the Revision History of an SRS Project
Procedure
Change the SRS Template that is Defined for an SRS Category in an SRS Project
Procedure
Compare the Revision Records of an SRS Project
Procedure
Link an SRS Project to Instrumented Function, SIL Analysis, Protective Loop, and Logic Solver
Before You Begin
Procedure
- Link an SRS Project to Instrumented Function
- Link an SRS Project to SIL Analysis
- Link an SRS Project to Protective Loop
- Link an SRS Project to Logic Solver