Checkpoints
About Route Checkpoints
Checkpoints are the stops along a Route at which a user will need to record a reading. For each Checkpoint that you want to include in a Route, you will need to add one Measurement Location or Lubrication Requirement to the Route. The order in which the Checkpoint nodes are displayed in the left pane represents the order in which the Checkpoints will appear to the user on the mobile device. Additionally, you can change the order in which the Checkpoint nodes are displayed.
Details
A Checkpoint can be linked to the following:
One Route as a successor | In the left pane, a node representing a successor Checkpoint that is linked to the Route appears directly below the Route node. When a Route is initially opened, and a Checkpoint is selected, the Identification tab is displayed. If you select a different tab on a Checkpoint (Schedule, Readings, Reference Documents), and then select a different Checkpoint, the same tab appears for the new Checkpoint. |
Checkpoint conditions as a predecessor or successor | In the left pane, a node representing a successor Checkpoint that is linked to a Checkpoint condition appears below the Checkpoint condition node representing that Checkpoint condition. Likewise, a node representing a predecessor Checkpoint record that is linked to a Checkpoint condition record is displayed. When a Route is initially opened, and a Checkpoint condition is selected, the Identification tab is displayed. If you select a different tab on a Checkpoint condition (Readings or Reference Documents), and then select a different Checkpoint condition, the previous tab appears for the new Checkpoint condition. If you select the Schedule tab for a Checkpoint, and then select a Checkpoint condition, the Identification tab appears as there is no Schedule tab for a Checkpoint condition. If you select a condition or use search, then the next time a Checkpoint is selected, the same tab is displayed. |
Checkpoint records that appear below a Checkpoint condition record will appear to a device user only if the condition defined in the Checkpoint condition is met.
When you add a Checkpoint record to a Route, the new node that appears in the left pane for that record will appear in a location that is relevant to the currently selected node. Before you create a Checkpoint record, use the following guidelines to determine which node to select in the left pane so that the new node will appear in the desired location:
- If you want the new Checkpoint node to appear below a Checkpoint node, select that Checkpoint node.
- If you want the new Checkpoint node to appear below a Checkpoint condition node, select that Checkpoint condition node.
- If you want the new Checkpoint record to appear below the last node in the pane, select that Route node.
When you are adding Checkpoint records to a Route, keep in mind that the values in the record define the Checkpoint and directly represents what the device user will see on the mobile device. More specifically, the values stored in some Checkpoint family fields are displayed directly on the Rounds Data Collection page when you are recording a reading for the corresponding Checkpoint.
About Route Checkpoint Arrangement
The order in which the Checkpoints are presented on the device corresponds to the order in which the Checkpoint nodes appear in the left pane when viewing a route in Route Designer.
In order to maximize system performance, sequence information for each Route is stored as a single record in a database table , not on the route, Checkpoint, or condition records themselves. When changing the sequence of a Route, the value representing the Route sequence in the supporting database table will be updated automatically to reflect the current location of each node. In order to support Rounds on Windows Mobile devices — which use Catalog queries - sequence information is also stored as Rounds Sequence Information records.
Selecting the Save Route Sequence button on a Route after reordering allows the Route sequence to be immediately reflected when you download the route to a handheld. Otherwise, Rounds Sequence Information records will be updated after the route has been closed or on a defined schedule.
Checkpoint represented by a Measurement Location
A Checkpoint represented by a Measurement Location with the Sequence value 1 will appear before a Checkpoint represented by a Measurement Location with the Sequence value 2. On the Measurement Location datasheet, the Sequence field is disabled and populated automatically by the APM system, based upon the current location of that Measurement Location node in the left pane.
You can use the left pane to sequence the Measurement Location nodes according to the order in which you want the Checkpoints to appear to a user on the mobile device. We recommend that you sequence the Route by arranging Measurement Location nodes in an order that corresponds to the proximity of the associated equipment and locations. For example, suppose you want to perform a visual inspection of a pump. You will want to create Measurement Locations that represent each Checkpoint on the pump that you will need to visually inspect. Further, you will want to arrange the Measurement Location nodes in the order in which the user should conduct the visual inspection. For example, you may want the user to start at the back of the pump and move towards the front.
Measurement Locations are sequenced automatically starting with 1, based upon the record to which they are linked as a successor. In other words, all the Measurement Locations that are linked directly to the Route as successors will be numbered 1, 2, 3, and 4 and all the Measurement Locations that are linked to Checkpoint conditions will be numbered as 1, 2, 3, and 4 within that condition.
Consider the following image, which shows:
- Four Measurement Location nodes that are positioned directly below the Route node. These route-level Checkpoints are numbered 1 through 4.
- Two Checkpoint condition nodes that are positioned directly below the Measurement Location node (ACHE 001~General Check). These Checkpoint condition nodes are numbered 2.1 and 2.2.
-
Four Measurement Location nodes that are positioned directly below two Checkpoint conditions.
The Measurement Location nodes under 2.1 If General Check is Ok then: are numbered 2.1.1 and 2.1.2. The Measurement Location nodes under 2.2 If General Check is Not Ok then: are numbered 2.2.1 and 2.2.2.
About The Node Pin Board
Using the Node Pin Board pane, you can use the drag-and-drop method to move one or more locations, or conditions from the Route to the Node Pin Board pane, and then later move them to new Checkpoints or remove them from the Route.
- Checkpoints or conditions on the Node Pin Board pane include any child Checkpoints or conditions that are linked to the parent node.
- You will not be able to drag and drop an item until the dark blue insertion marker appears under the node where the item will be dropped.
- A Checkpoint that contains conditions and subsequent Checkpoints can be dragged and dropped as a single entity. However, if you want to drag two top-level Checkpoints, you have to drag and drop each one separately.
- When a condition is deleted from the Route, the Checkpoints and conditions that were successors to that condition will be moved to the Node Pin Board pane.
-
You cannot drag and drop an Equipment or Functional Location to the Node Pin Board pane. However, if you remove an asset group from the Route, the associated Checkpoints, including any related conditions and subsequent Checkpoints, will be moved to the Node Pin Board.
About Alerts Based on Measurement Location Records
If you want device users to receive alerts on a device when they record reading values that meet certain criteria, you can define the criteria in the Limit Values section of the default datasheet for the Measurement Location family. You can configure alerts for either character readings or for numeric readings, depending on the value stored in the ML Type field of the Measurement Location.
About Alerts for Character Readings

Notice that the Character column contains the values that will cause an alert to appear: Leak, Vibration and Noise. The Message column contains the message that will be displayed for each alert, and the Action column contains the values that will be available in the Action list on the Rounds Data Collection screen.
Example: Pump Check Checkpoint
The following image shows what the Pump Check Checkpoint looks like on the device with the Reading drop-down list box.
If you enter a reading value of Leak for this Checkpoint, the text Create Maintenance Recommendation should be displayed on the device, as indicated by the Message column in the corresponding Measurement Location. This value is shown in the image of the Limit Values section. The following image shows what the alert for the reading value Leak looks like on the device.
The Action Taken drop-down list would contain the values indicated by the Action Values tab list column.
About Configuring Alerts for Numeric Readings
When a Measurement Location requires a numeric reading value, you can configure alerts that will appear when the reading value equals a specified value or falls between a certain range of values, depending on the following conditions:
- If allowable values are defined for a Measurement Location where the ML Type field contains the value Numeric, you can configure alerts that will appear when the readings are equal to those values.
- If allowable values are not defined in a Measurement Location where the ML Type field contains the value Numeric, you can configure alerts that will appear when the readings fall within a range of values.
Example: Temperature Check Checkpoint
Suppose a Checkpoint requires a temperature check and accepts numeric reading values. If you do not define allowable values in the Identification section of the datasheet for Measurement Location, users can enter any reading value on the device. You might want to define these allowable values so that an alert will be sent if the temperature falls below a certain temperature or rises above a certain temperature.
In the following image, you can see that values have been defined for Upper Level 3, Upper Level 2, Upper Level 1, Lower Level 1, Lower Level 2, and Lower Level 3 limits.

The Upper Level 3 value of 750 indicates that if a reading value is greater than or equal to 750, an alert will be displayed with the message Extreme operating temp - shut down, as specified by the value in the Message cell.
When you are working with lower-level values, keep in mind that any reading that is less than or equal to the value will trigger the alert. Likewise, when working with upper-level values, keep in mind that any reading that is greater than or equal to the value will trigger the alert.
Example: Daily Temperature Readings
Suppose that you configure a Measurement Location with an Upper Level 2 value of 100 and an Upper Level 3 value of 200, and the message associated with the Upper Level 2 is "Pump stroke too high". If a device user enters a reading value of 185 at this Checkpoint, the following alert would appear.
In the list on the Action Values tab , you would also see the list of actions indicated by the values in the Action column for the corresponding Measurement Location. Device users can select one of these values to indicate which task was performed in response to the alert.
About Checkpoint Conditions
When you create a Checkpoint condition, its corresponding node will appear in the left pane below the predecessor Checkpoint node. If you want to add a Checkpoint condition node in a particular location (for example, between two Checkpoint condition nodes), you should select the Checkpoint condition node after which the new Checkpoint condition node should appear.
Depending upon the type of Checkpoint for which you are creating a condition (that is, character or numeric), the values that you define will vary.
- For Measurement Locations, the type of condition is determined by the value in the ML Type field in the predecessor Measurement Location. The value of this field can contain either Character or Numeric.
- For all types of Lubrication Requirements, the condition is based on the character reading values.
About Character Checkpoint Conditions
When you create a Checkpoint condition that is linked to a Measurement Location whose ML Type field contains the value Numeric, the following text appears on the Checkpoint condition node:
If <ML Category> <Relational Operator> <Reading Value> then:
…where:
- <ML Category> is the value stored in the Category field in the Measurement Location. This value is populated automatically after you create the Checkpoint condition and is used to identify the predecessor Measurement Location whose reading value may trigger the additional Checkpoints to appear.
- <Relational Operator> is the operator (that is, is or is not) that you select in the Select Relation drop-down list box when creating a Checkpoint condition. By default, the operator, is, appears in the Select Relation drop-down list box.
- <Reading Value> is the value that you select in the Select Value drop-down list box in the workspace for the Checkpoint condition.
The following image shows an example of what a character Checkpoint condition record looks when it is selected in the left pane.
In this image, you can see that Filter Check is the ML Category and Leak is the reading value.
About Numeric Checkpoint Conditions
When you create a Checkpoint condition that is linked to a Measurement Location whose ML Type field contains the value Character, the following text appears on the Checkpoint condition node:
If <ML Category> <=><Reading Value> then:
... where:
- <ML Category> is the value stored in the Category field in the Measurement Location. This value is populated automatically after you create the Checkpoint condition and is used to identify the predecessor Measurement Location whose reading value may trigger the additional Checkpoints to appear.
- <=> is the quantifier (i.e., <, <=, =, >=, or >) selected in the Select Relation list in the workspace. This specifies the parameters of the condition when used in conjunction with the value in the <Reading Value> cell. The default value is = (equals).
- <Reading Value> is the value entered in the Select Value cell in the workspace.
In other words, you can specify that if the reading value is equal to the value in the Reading Value cell, the successor Checkpoint should appear.
The following image shows an example of what a numeric Checkpoint condition looks like when it is selected in the left pane.
In this image, you can see that:
- Pump Stroke Check is the ML Category.
- <= is the quantifier.
- 500 is the Reading Value.
About Lubrication Checkpoint Conditions
When you create a Checkpoint condition that is linked to a Lubrication Requirement, the following text appears on the Checkpoint condition node:
If <LR Type> is <Reading Value> then:
...where:
- <LR Type> is the value stored in the LR Type field in the Lubrication Requirement. This value is populated automatically after you create the Checkpoint condition and is used to identify the type of predecessor Lubrication Requirement whose character reading value may trigger the additional Checkpoints to appear. There are three types of Lubrication Requirement:
- Check Off
- Change Out
- Tracking
- <Reading Value> is the value that you select from the Select Value list in the workspace for the Checkpoint condition. There are two available character reading values for a Lubrication Requirement:
- Done
- Skip
The following image shows an example of what a lubrication Checkpoint condition record looks when it is selected in the left pane.

In this image, you can see that Check Off is the LR Type.
About Conditions for Routes
When a device user is executing the Checkpoints along a Route, if the reading value that is taken for a Checkpoint indicates further investigation is needed, you may want the device user to see additional Checkpoints on the device and record reading values for those additional Checkpoints. To accomplish this, you can add conditions to the Checkpoints on the Route. A condition allows you to add logic to the Route to specify that when a particular reading value is recorded for a Checkpoint, additional Checkpoints should be displayed to the device user.
Details
A condition identifies which Checkpoint should appear on the device if the user enters a specific reading value for the previous Checkpoint and defines:
- The initial Checkpoint whose reading value should trigger a subsequent Checkpoint.
- The specific reading value that should trigger another Checkpoint.
- The subsequent Checkpoint that should be triggered by that reading value.
In the APM database, a single condition is represented by:
- One Checkpoint that identifies the initial Checkpoint.
- One Checkpoint condition that identifies the specific reading value.
- One or many Checkpoints that identify the subsequent Checkpoints.
In the left pane, Checkpoint condition nodes are displayed in the context of the Checkpoint node representing the initial and subsequent Checkpoints. Specifically, the Checkpoint condition node appears below the Checkpoint representing the initial Checkpoint. Likewise, the Checkpoint node representing the subsequent Checkpoint appears below the Checkpoint condition node.
The following image shows how the Checkpoint and Checkpoint conditions will be linked to one another to define a condition.

A single Checkpoint condition can be linked as a successor to only one Checkpoint. A Checkpoint, however, can be linked to multiple successor Checkpoint conditions. Likewise, a Checkpoint condition can be linked to multiple successor Checkpoints.
Access a Checkpoint
Procedure
Create a Checkpoints Using a Blank Datasheet
Create a Checkpoint from a Template
Add an Existing Checkpoint to a Route
Manually Assign a Scan ID to a Measurement Location
Procedure
Results
- After assigning the Scan ID, when you collect data, if you scan the ML, the ML record will open automatically.
Modify a Checkpoint
Procedure
Use the Node Pin Board
About This Task
Procedure
Add a Condition to a Route for a Character Measurement Location
About This Task
This topic describes how to create a Checkpoint condition and add it to a Route in one of two ways:
- As a successor to a Measurement Location whose ML Type value is character
- As a predecessor to a Measurement Location
Procedure
Add a Condition to a Route for a Numeric Measurement Location
About This Task
This topic describes how to create a Checkpoint condition and add it to a Route:
- As a successor to a Measurement Location whose ML Type value is numeric.
- As a predecessor to a Measurement Location.
Procedure
Add a Condition to a Route for a Lubrication Requirement
About This Task
This topic describes how to create a Checkpoint condition and add it to a Route:
- As a successor to a Lubrication Requirement for all types of Lubrication Requirements.
- As a predecessor to a Lubrication Requirement.
Procedure
Add an Image to a Checkpoint
About This Task
This topic describes how to add an image to a Checkpoint that will appear when you access the Checkpoint in Rounds Data Collection.
Procedure
Results
- The Checkpoint is saved.
-
The specified image appears in the workspace for the Checkpoint in Rounds Data Collection.
Tip: In Rounds Data Collection, you can select the image to display it in full screen.
A Checkpoint with an Image in Rounds Data Collection
Example:Suppose that you have a Route containing a Checkpoint to inspect flanges on a pipe. You can add an image of the flanges to that Checkpoint in Rounds Designer so that it can be easily referenced while collecting readings in Rounds Data Collection, as shown in the following image.
Configure Alerts
Before You Begin
About This Task
If you want device users to receive alerts on a device when they record reading values that meet certain criteria, you can define the criteria in the Limit Values section of the Checkpoint datasheet. You can configure alerts for either character readings or for numeric readings, depending on the value stored in the ML Type field of the Measurement Location.