Data Loaders
About the Inspection Management (IM) Data Loaders
The following Data Loaders are available in Inspection Management:
- Inspection Management (IM) Assets Data Loader
- Inspection Management (IM) Functional Location Data Loader
Throughout the documentation, these Data Loaders are collectively called the Inspection Management (IM) Data Loaders. You can use them to implement Inspection Management when you have inspection data in a legacy system. To import data using these Data Loaders, APM provides the following Excel templates:
- Inspection Management (IM) Assets.xlsx: Using this Data Loader, you can create or update Inspections and related records that are linked to Equipment records.
- Inspection Management (IM) Functional Location.xlsx: Using this Data Loader, you can create or update Inspections and related records that are linked to Functional Location records.
The data from the templates will be imported into APM using the corresponding Data Loaders.
- The Excel templates are referred to throughout this documentation as the data loader workbooks.
- Do not add any European Inspection related fields to the Data Loader templates.
You can use the data loader workbooks to create or update records in the following Inspection families:
- Inspection Confidence Evaluation
- Inspection Profile
- Inspection Method
- Inspection Task
- Inspection (i.e., Bundle Inspection, Full Inspection, General Inspection, Pressure Test Inspection, and all types of Checklists)
- General Finding
- Bundle Sub-Inspection
- Pressure Test Sub-Inspection
- Inspection Recommendation
- Reference Document
Using the data loader workbooks, you can also create:
- Records that represent archived Inspections (i.e., inspections that have been completed and approved in the past). Since archived Inspections will be locked after creation, they cannot be updated using the data loader workbooks.
- Records of a custom sub inspection family that you may have created.
The data on the (Picklist) worksheet is not loaded when you load data.
About the Inspection Management (IM) Data Loaders Requirements
This documentation assumes that your organization has fully completed the deployment of the Inspection Management module. The Inspection Management (IM) Data Loaders should only be used after the Inspection Management module has been implemented, and you have defined Site References, Functional Locations, and assets (Equipment records) for your organization.
Human Resources and Resource Roles
The Inspection Management (IM) Data Loaders expect that individuals in your organization who will be performing and reviewing Inspections have one or more of the following Resource Role records linked to their Human Resource records:
- Inspection Supervisor
- Inspector
Certain privileges are required to complete a data load based on to whether inspections are (Active or Archived and the State of the inspection Draft, Pending Approval, or Approved). Persons belonging to either the MI Inspection or the Data Loader User Security Group must:
... have the following Resource Role(s): | ...with inspections that are: | ...and inspections in the following State: | Notes |
---|---|---|---|
None | Active | Draft | None |
Inspector or Contract Inspector Note: The Contract Inspector must be assigned as a Team Member to request approval on the Inspection Report by updating the State field. | Active | Pending Approval | None |
Inspector and Inspection Supervisor | Archived | Approved | The Inspection Lock and the Final Inspection Lock are set to true. |
Security Settings
The Security User performing the data load operation must be associated with either the MI Data Loader User or MI Data Loader Admin Security Role, and must also be associated with the MI Inspection Security Group, or a Security Role that is associated with this Security Group.
About the Inspection Management (IM) Data Loaders Inspection Types
The Inspection Management (IM) Data Loaders can be used to load two different types of Inspections:
-
Active Inspections: Inspections that are still in the process of being completed or reviewed. After you load data, you can use the Inspection Management Bulk Approval feature to approve active inspections. Note:
- If an inspection is currently downloaded for Inspection Field Data Collection, it cannot be updated through the data loader until it has been synced back.
- If the Use State Management for Inspection Recommendations check box in Application Settings is selected, Active Inspection Recommendations are loaded in the Proposed state. If it is cleared, Active Inspection Recommendations are loaded in the Created status.
-
Archived Inspections: Inspections that have been reviewed, locked, and archived. Because of the nature of approving archived inspections, it is best for one person to perform this function. In the data loader workbooks, archived Inspections are those that have both the Inspection Lock and Final Inspection Lock fields set to True, and the State field set to Approved. When an archived Inspection is loaded, the Inspection Report Owner and Reviewer’s Name fields will be set to the name of the user performing the data load. Note: If the Use State Management for Inspection Recommendations check box in Application Settings is selected, Archived Inspection Recommendations are loaded in the Completed state. If it is cleared, Archived Inspection Recommendations are loaded in the Implemented status.
About the Inspection Management (IM) Data Loaders Data Model
This topic has been intentionally excluded from the APM product documentation website. This topic is available to you via the product documentation that is provided within the APM system.
About the Inspection Management (IM) Data Loaders General Loading Strategy
Prerequisites
- For Oracle databases, valid cell values are case-sensitive.
- The data loader workbook contains sample data in each column. It is only for your reference. You must remove this data before using the data loader workbook.
Best Practices
When importing data using the Inspection Management (IM) Data Loaders, you must use the following best practices:
- ID fields (the second row on each worksheet) must not include special characters or spaces.
- Columns (including columns representing custom fields) on the worksheets should be formatted as Text.
-
When loading archived Inspections, you do not need to set values for the Inspection Report Owner and Reviewer’s Name cells. These fields will be set automatically to the name of the user who loads the data.
- The supported date formats, time zone, and units of measure will be based on the user's settings.
- When creating ID numbers for loading inspection data, choose unique values.
- The value in the Inspection Reference field must be unique.
- State ID rules are not executed when transitioning states of an inspection when it is uploaded using a data loader Excel. If there are any fields that are set as part of the state transition rule logic, those should be included as part of the Excel. For example, in a baseline configuration for an inspection being loaded in the Pending Approval state, if it is expected that the Inspection Lock field is set to True due to the state, the field should be marked as True in the Excel.
Load Sequence
The Inspection Management data load is performed in a specific sequence in order to create all necessary relationships between records:
- The first step of the load sequence differs based on whether you are using the Inspection Management (IM) Assets Data Loader or the Inspection Management (IM) Functional Location Data Loader.
If using the Inspection Management (IM) Assets Data Loader, the Assets worksheet is processed. An existing asset will be looked up based on values in the Equipment ID (MI_EQUIP000_EQUIP_ID_C), CMMS System (MI_EQUIP000_SAP_SYSTEM_C), and, if provided, Equipment Technical Number (MI_EQUIP000_EQUIP_TECH_NBR_C) cells.
If using the Inspection Management (IM) Functional Location Data Loader, the Functional_Location worksheet is processed. An existing Functional Location will be looked up based on values in the Functional Location ID (MI_FNCLOC00_FNC_LOC_C) and CMMS System (MI_FNCLOC00_SAP_SYSTEM_C) cells.
If an Asset or Functional Location specified on the respective worksheets does not exist, it will be skipped, along with all entries in the subsequent worksheets corresponding to that Asset or Functional Location.
- The Inspection_Profile worksheet is processed. For each row based on the cells specified in step 1, an Inspection Profile is looked up. If the Asset or Functional Location does not have a corresponding Inspection Profile, a new record will be created and linked.
- The Inspection_Method worksheet is processed. The assets or Functional Locations from step 1 and the Inspection Profiles from step 2 are considered, in addition to the following columns on the worksheet: Item Category (MI_PROFINSP_ITEM_CAT_C), Item ID (MI_PROFINSP_ITEM_ID_C), Method Category (MI_INSPMETH_ITEM_CAT_C), Method ID (MI_INSPMETH_ITEM_ID_C), and (only for assets) RBI Degradation Mechanism (MI_INSPMETH_DAMAGE_MECH_C).
- If a corresponding Inspection Method is not found, a new Inspection Method record will be created. Otherwise, the record will be updated The Inspection_Task worksheet is processed. The assets or Functional Locations from step 1 are considered as well as the following columns on the worksheet: Task ID (MI_TASK_ID), Reoccurring (MI_TASK_REOCC_FLG), and Override Interval (MI_TASK_OVERRIDE_INTER_F).
If the Reoccurring cell is set to True, the Next Date cell cannot be specified because the task is reoccurring. As a result, the Next Date value will be automatically calculated.
If the Override Interval cell is set to False, the setting of the Desired Interval cell by the data loader will not occur and the Desired Interval will be set to 0. Therefore, the Override Interval cell cannot be set to False.
If the Override Interval cell is set to False, but the value in the Desired Interval cell is less than the value in the Minimum Interval cell, the Desired Interval will be set to the value of Minimum Interval.
If the Reoccurring cell of the task is set to False, the Last Date and the Desired Interval cells cannot be specified. For tasks that are not set to reoccur, the following cells will not be copied from the data loader spreadsheet and they will have the following default settings:
- The Last Date cell will be empty.
-
The Desired Interval cell will be set to 0.
If logical cells (i.e. Override Interval, Reoccurring) do not have values, they will be set to True by default.
- The Inspections worksheet is processed. For each row based on the cells specified in step 1, as well as the Inspection Reference (MI_EVENT_ID) column, an Inspection. If no corresponding Inspection record is found, then a new record is created. Otherwise, the record will be updated.
If the State cell is set to Approved and the Final Inspection Lock (MI_INSP_001_LOCK_FINAL_L) cell is set to True, the record will be considered an Archived Inspection. The Reviewer and Inspection Owner fields are automatically set to the user performing the data load.
If the Inspection Task Complete field has been added as a column to the worksheet, and if values have been provided, an error message will be added to the log, and data in the columns will be skipped.
State is used for Inspection approval process instead of Inspection Document Status. If a customer adds both the State (MI_SM_STATE_ID_C) and Inspection Document Status (MI_INSP_001_STATUS_INSP_C) in the excel, a warning message is logged, and the State field is used to process the record.
If an existing Inspection is being updated via the data load, but the Inspection Lock field for the record is set to True, and:
-
...you are not the user designated in the Inspection Report Owner field, an error message will be added to the log and the Inspection will not be updated.
-or-
-
...you are the user designated in the Inspection Report Owner field, but the data being loaded via the Excel workbook does not set the corresponding Inspection Lock cell to False, an error message will be added to the log and the Inspection will not be updated.
-
- The General_Finding worksheet is processed. Based on the fields in steps 1 and 5, and the Inspection Profile and Method, a General Finding record will be looked up. If the record is not found, then a new record is created. Otherwise, the record will be updated.
- The Inspection_Recommendation worksheet is processed. Based on the fields in steps 1 and 5, and the Recommendation ID (MI_REC_ID) column, an Inspection Recommendation is looked up. If a corresponding Inspection Recommendation is not found, then a new record is created. Otherwise, the record will be updated.
If the Inspection Recommendation record is associated with an Archived Inspection, then the Author Name and Reviewer Name fields for the Inspection Recommendation record will be set to the user performing the data load.
- The Reference_Document worksheet is processed. Based on the field in step 5, and the Reference Document ID (CTIT_ID) column, a Reference Document is looked up. If a corresponding Reference Document is not found, then a new record is created. Otherwise, the record will be updated.
- The Bundle_Sub_Inspection, the Pres_Test_Sub_Inspection, and the Inspection_Confidence Worksheets are processed. Based on the field in step 5, and the Inspection Reference (MI_EVENT_SUB_INSP_ID) column, the related inspection is looked up. If a corresponding related sub-inspection record is not found, a new record will be created.
Currently, the sub-inspection families that are supported by the Inspection Management (IM) Data Loaders are the Bundle Sub-Inspection and Pressure Test Sub-Inspection families.
For the Bundle Sub-Inspection family, there are several combinations of column values which you cannot load and the combination of these column values will result in an error:
-
An error will be issued in the log if the value of the Action This Inspection column is set to NO ACTION and any of the following columns have a value:
- Tubes Plugged During This Inspection
- Tubes (Plugged At Start) Replaced
-
Tubes (Not Previously Plugged) Replaced
-
An error will be issued in the log if the value in the Action This Inspection cell is set to TUBES PLUGGED, TOTAL RETUBE, or BUNDLE REPLACED and any of the following columns are set to:
-
Tubes (Plugged At Start) Replaced
-
Tubes (Not Previously Plugged) Replaced
- The column header for the sub-inspection Reference value will be different for each sub-inspection family, but will be similar to <Sub-Inspection Family Name> Reference.
- The value in the sub-inspection reference column will be stored in the Inspection Reference column of each created Sub-Inspection record. That column will be used for lookup when performing further loads.
-
The sub-inspection will be updated with the data given from the Inspection Management (IM) Data Loaders Template.
-
-
Since a relationship definition does not exist between the Bundle Sub-Inspection family and the General Inspection family, an error will be issued.
Note: If the relationship definition is added between the Bundle Sub-Inspection family and the General Inspection family, the Bundle Sub Inspection family will load.
-
About the Inspection Management (IM) Data Loaders Workbook Layout and Use
- Inspection Management (IM) Assets.xlsx (for Inspections related to Equipment records)
- Inspection Management (IM) Functional Location.xlsx (for Inspections related to Functional Location records)
You must use these workbooks to load the data. You can modify the Excel workbooks to include custom fields used by your organization. Generally, your organization will use one of the two workbooks, but not both.
The following table provides a list of worksheets that are included in the data loader workbooks. Unless otherwise specified, the worksheets appear in both the workbooks.
Worksheet | Description |
---|---|
Assets | This worksheet is used to specify existing Equipment records to which Inspections and related records will be linked. This worksheet appears only in the Inspection Management (IM) Assets Data Loader workbook. |
Functional_Location | This worksheet is used to specify existing Functional Location records to which Inspections and related records will be linked. This worksheet appears only in the Inspection Management (IM) Functional Location Data Loader workbook. |
Inspection_Profile | This worksheet is used to specify Inspection Profile records that you want to create or update. |
Inspection_Method | This worksheet is used to specify Inspection Method records that you want to create or update. |
Inspection_Task | This worksheet is used to specify Inspection Task records that you want to create or update. |
Inspections | This worksheet is used to specify the following records:
|
Inspection_Confidence_Eval | This worksheet is used to specify Inspection Confidence Evaluation records that you want to create or update. |
Bundle_Sub_Inspection | This worksheet is used to specify Bundle Sub-Inspection records that you want to create or update. |
Press_Test_Sub_Inspection | This worksheet is used to specify Pressure Test Sub-Inspection records that you want to create or update. |
General_Finding | This worksheet is used to specify General Finding records that you want to create or update. |
Custom_Sub_Inspection | If you have created a custom sub inspection family, this worksheet is used to specify the custom sub inspection records that you want to create or update. |
Inspection_Recommendation | This worksheet is used to specify Inspection Recommendation records that you want to create or update. |
Reference_Document | This worksheet is used to specify Reference Document records that you want to create or update. |
(Picklist) | This worksheet contains a list of valid values that you can enter in each column (as applicable) in the aforementioned worksheets. When you load data using the data loader, the data on this worksheet is not loaded. |
Color Coding
Certain columns on the worksheets have different functions and requirements. To illustrate this, certain columns are color-coded. The following table lists the colors and what they represent.
Color | Description | Comments |
---|---|---|
Grey | Lookup Fields | Indicates columns that contain values that are used by the Inspection Management (IM) Data Loaders to look up and create records. If these columns are removed from the worksheets, the data load will fail. While the worksheets require that these columns be present, values are not necessarily required in these columns. |
Red | Fields Required for Saving Records | Indicates columns that contain values that are required to save the record. |
Blue | Recommended Fields | Indicates columns that, according to APM Best Practice for Inspection Management, should contain values. |
Green | Custom Fields | Indicates columns in which you can specify custom fields. |
Limitations
The Inspection Management (IM) Data Loaders have the following limitations:
- The values that you enter in the data loader workbooks are case-sensitive.
-
When you use the data loader to update Inspection Management families:
-
If a cell contains data, the value in the corresponding field will be updated in the database.
-
If a cell is blank, the value in the corresponding field will not be updated with a blank value in the database. The value that previously existed in the field is retained.
-
-
If you reimport data, the records that have been created by the Data Loaders will be updated. Therefore, while reimporting data, if you remove the data for a field in the data loader workbooks, the value for the corresponding field in APM will be either a default value or blank.
Tip: If you do not want to update a field value, you can remove the corresponding column from the data loader workbooks. You cannot, however, remove columns that correspond to required fields.
Assets Worksheet
On the Assets worksheet, you can specify assets to which you want to link Inspections and related records. The columns that appear on this worksheet also appear on every subsequent worksheet, and are used to identify the records that will be linked, directly or indirectly, to the assets. This worksheet only appears in the Inspection Management (IM) Assets Data Loader workbook.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | A value is required in at least one cell. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C | Character (255) | If the Equipment record for an asset has a value in the CMMS System field, you must enter that value in this column. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | If the CMMS System column contains a value, and the Equipment record for the asset has a value in the Equipment Technical Number field, you must enter that value in this column. If the CMMS System column does not contain a value, this column can be blank, even if the Equipment record contains a value for the Equipment Technical Number field. |
Functional_Location Worksheet
On the Functional_Location worksheet, you can specify Functional Location records to which you want to link Inspections and related records. The columns that appear on this worksheet also appear on every subsequent worksheet, and are used to identify the records that will be linked, directly or indirectly, to the Functional Locations. This worksheet appears only in the Inspection Management (IM) Functional Location Data Loader workbook.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | A value is required in at least one cell. |
CMMS System | MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | If the CMMS System field in the Functional Location record contains a value, you must enter that value in this column. |
Inspection_Profile Worksheet
On the Inspection_Profile worksheet, you can specify Inspection Profile records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Item Category | MI_PROFINSP_ITEM_CAT_C | Character (50) | A value is required. The combination of values in the Item Category and Item ID columns must be unique per asset. This column must only contain System Code IDs from the MI_INSPECTION_PROFILE_CATEGORY System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Item ID | MI_PROFINSP_ITEM_ID_C | Character (255) | A value is required. The combination of values in the Item Category and Item ID columns must be unique per asset. |
Item Description | MI_PROFINSP_ITEM_DESC_C | Text | None |
RBI Component | MI_PROFINSP_COMPONENT_C | Character (250) | This column must only contain the Entity ID of an existing Criticality RBI Component record that is linked to the same asset or Functional Location as the Inspection Profile. |
RBI Component Family | MI_PROFINSP_COMP_FAM_C | Character (100) | This column must only contain the Family name of the Criticality RBI Component specified in the RBI Component column (e.g., Criticality RBI Component - Piping). This column appears only in the Inspection Management (IM) Assets Data Loader workbook. |
Sequence | MI_PROFINSP_SEQUENCE_N | Numeric | None |
Inspection_Method Worksheet
On the Inspection_Method worksheet, you can specify Inspection Method records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Item Category | MI_PROFINSP_ITEM_CAT_C | Character (50) | Values in this column must match the values entered on the Inspection_Profile worksheet, if they exist. You can link multiple records to the same Inspection Profile. |
Item ID | MI_PROFINSP_ITEM_ID_C | Character (255) | Values in this column must match the values entered on the Inspection_Profile worksheet, if they exist. You can link multiple records to the same Inspection Profile. |
Method Category | MI_INSPMETH_ITEM_CAT_C | Character (100) | A value is required. The combination of values in the Method Category, Method ID, and RBI Degradation Mechanism columns must be unique per Inspection Profile. This column must only contain one of the System Code IDs from the MI_INSPECTION_METHOD_CATEGORY System Code Table. To verify which options are acceptable in your APM system, via Configuration Manager, refer to the appropriate table. |
Method ID | MI_INSPMETH_ITEM_ID_C | Character (255) | A value is required. The combination of values in the Method Category, Method ID, and RBI Degradation Mechanism columns must be unique per Inspection Profile. |
RBI Degradation Mechanism | MI_INSPMETH_DAMAGE_MECH_C | Character (255) | A value is required. This column must only contain the Entity ID of a Potential Degradation Mechanism that is linked to the Criticality RBI Component specified in the corresponding RBI Component column on the Inspection_Profile worksheet. The combination of values in the Method Category, Method ID, and RBI Degradation Mechanism columns must be unique per Inspection Profile. Important: This column appears only in the Inspection Management (IM) Assets Data Loader workbook, and should not be included in the Inspection Management (IM) Functional Location Data Loader workbook. |
Description | MI_INSPMETH_ITEM_DESC_C | Character (1000) | None |
Inspection_Task Worksheet
On the Inspection_Task worksheet, you can specify Inspection Task records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Task ID | MI_TASK_ID | Numeric | A value is required and must be unique. This value identifies the Inspection Task. |
Task Type | MI_TASK_TASK_TYPE_CHR | Character (255) | None |
Task Description | MI_TASK_DESC_TX | Text | None |
Task Details | MI_TASK_DETAILS_T | Text | None |
Last Date | MI_TASK_LAST_DATE_DT | Date | Enter a value in the following format: YYYY-MM-DD hh:mm:ss |
Override Interval | MI_TASK_OVERRIDE_INTER_F | Boolean | Enter True or False. |
Desired Interval | MI_TASK_DESIR_INTER_NBR | Numeric | None |
Next Date | MI_TASK_NEXT_DATE_DT | Date | Enter a value in the following format: YYYY-MM-DD hh:mm:ss |
Next Date Basis | MI_TASK_NEXT_DATE_BASIS_C | Character (1000) | None |
Coverage | MI_TASK_COVER_NBR | Numeric | None |
Task Assigned To | MI_TASK_ASSGN_TO_C | Character (50) | None |
Reoccurring | MI_TASK_REOCC_FLG | Boolean | Enter True or False. You can enter a value in this column only if you want to create an Inspection Task. If, however, you want to modify an Inspection Task using the data loader workbook, you cannot modify the value in this column. |
Unconstrain Min/Max Dates | MI_TASK_UNCONSTR_MN_MX_DT_FLG | Boolean | Enter True or False. |
Min Interval | MI_TASK_MIN_INTER_NBR | Numeric | None |
Max Interval | MI_TASK_MAX_INTER_NBR | Numeric | None |
Inspection Document Type | MI_TASK_INSP_INSPTYPE_FMLYID_C | Character (50) | None |
Inspections Worksheet
On the Inspections worksheet, you can specify the following types of Inspections that you want to create or update:
- Bundle Inspection
- All types of Checklists (e.g., API 510 External Checklist, ILI Checklist)
- Full Inspection
- General Inspection
- Pressure Test Inspection
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | A value is required. If the value in the Use System Generated ID column is False (or if the column is blank), then the value in this column must be unique. If the value in the Use System Generated ID column is True, then, after you load data, the value in this column is not used to populate the Inspection Reference field in the Inspection. Instead, a system-generated value is used to populate the field. In this case, the value in this column is used only to identify the records that must be linked to the Inspection. |
Use System Generated ID | MI_SYS_GEN_ID | Logical | Enter True or False. If you enter False (or leave this column blank), after you load data, the value in the Inspection Reference column is used to populate the Inspection Reference field in the Inspection. The default value is False. If you enter True, after you load data, the value in the Inspection Reference field in the Inspection is populated with a system-generated value. In this case, even if you enter a value in the Inspection Reference column, it is not used to populate the field. If you want to use the data loader workbooks to modify an Inspection, the value in this column must be False (or you can leave this column blank). If, however, the value in this column is True, then, after you load data, the Inspection is not modified. Instead, a new Inspection is created. |
Family ID | FMLY_ID | Character (255) | Values in this column are used to identify the type of the Inspection record that you want to create or update. In addition to the values specified on the (Picklist) worksheet, if you want to enter the family ID of a custom inspection family that you created, ensure that the family is linked to the Equipment or Functional Location family using the Has Inspections relationship family. |
Inspection Headline | MI_EVENT_SHRT_DSC_CHR | Character (255) | None |
Commencement Date | MI_EVENT_STRT_DT | Date | Enter a value in the following format: YYYY-MM-DD hh:mm:ss |
Completion Date | MI_EVENT_END_DT | Date | Enter a value in the following format: YYYY-MM-DD hh:mm:ss |
Tasks Addressed | MI_EVENT_TASKKEYS_C | Character (1000) | Enter a list of Entity Keys or Task IDs of Inspection Tasks, separated by commas. You can enter up to 20 values in each cell. |
Equipment Operating State | MI_INSP_001_STATE_EQUIP_OP_C | Character (50) | This column must only contain the System Code IDs from the MI_EQUIP_OP_STATE System Code Table. If the system code table has been customized, the valid values could be different. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Reason for Inspection | MI_INSP_001_REASON_C | Character (50) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Inspection Summary | MI_EVENT_LNG_DSC_TX | Text | None |
Inspection Report Owner | MI_INSP_001_NAME_INSPECTOR_C | Character (255) | The value in this column must match an existing Security User who is assigned the Inspector Resource Role. Enter value in the following format: <Last Name>, <First Name> ~ <User ID> |
State Id | MI_SM_STATE_ID_C | Character (50) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Inspection Lock | MI_INSP_001_LOCK_INSP_L | Boolean | Enter True or False. If the value in this column is True, and the Final Inspection Lock column is blank or False, the value in the Inspection Report Owner column must match the Security User who is loading the data. |
Reviewers Name | MI_INSP_001_NAME_REVIEWER_C | Character (255) | The value in this column must match an existing Security User who is assigned the Inspection Supervisor Resource Role. Enter value in the following format: <Last Name>, <First Name> ~ <User ID> |
Reviewers Comments | MI_INSP_001_COMMENTS_REVIEW_T | Text | None |
Final Inspection Lock | MI_INSP_001_LOCK_FINAL_L | Boolean | Enter True or False. If the value in this column and the Inspection Lock column is True, the Inspection Report Owner and Reviewer's Name fields for the record will be populated with the name of the user who is loading the data. |
Published | MI_INSP_001_PUBLISHED_L | Boolean | Enter True or False. |
Inspection Confidence Evaluation Reviewed | MI_INSP_001_ICE_COMP_F | Boolean | Enter True of False. If the value in this column is True, the Inspection Confidence Evaluation records are locked. You can update this field only if:
Note: This column is not a part of the baseline data loader template. If required, you can add this column to the Inspections worksheet. |
Inspection_Confidence_Eval Worksheet
On the Inspection_Confidence_Eval Worksheet, you can specify Inspection Confidence Evaluation records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System (only for Asset load) | MI_EQUIP000_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Value in this column must match the value in the Inspection Reference column of the parent inspection specified on the Inspections worksheet. |
Inspection Confidence ID | MI_EVENT_SUB_INSP_ID | Character (255) | Enter a unique value in the following format: <Inspection Reference>-<Sequence Number> |
RBI Component | MI_INSCONFEV_RBI_COMP_N | Numeric | Enter the Component field value of an existing RBI Component. The value in this field should be a valid RBI Component for the Asset that the Inspection is related to. Note: This column is not a part of the baseline data loader template. If required, you can add this column to the Inspection_Confidence_Eval worksheet. |
Filter DM | MI_INSCONFEV_FILT_DM_F | Boolean | Enter True or False. This field is required if the RBI Component field has a value. If the RBI Component field is blank, this field is ignored during loading. If the value in this column is True, and an RBI Component is specified, the degradation mechanism must belong to the specified RBI Component. Note: This column is not a part of the baseline data loader template. If required, you can add this column to the Inspection_Confidence_Eval worksheet. |
Degradation Mechanism | MI_INSP_001_DEG_MECH_C | Character (100) | This column must only contain the System Code IDs from the DEGRADATION_MECHANISM_TYPES System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Type of Inspection | MI_INSP_001_TYPE_C | Character (255) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Extent | MI_INSP_001_EXTENT_C | Character (1000) | This column must only contain System Code IDs from the MI_MI_INSPECTION_EXTENT System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Bundle_Sub_Inspection Worksheet
On the Bundle_Sub_Inspection worksheet, you can specify Bundle Sub-Inspection records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the Inspection Reference of the parent inspection specified on the Inspections worksheet. |
Bundle Sub Inspection Reference | MI_EVENT_SUB_INSP_ID | Character (255) | Values in this column are used to uniquely identify the Bundle Sub-Inspection. This field does not appear on the datasheet; however, it is used to uniquely identify the Bundle Sub-Inspection. |
Bundle Tag | MI_EVENT_ASST_ID_CHR | Character (255) | None |
Bundle Type | MI_INSPBUND_BUNDLE_TYPE_C | Character (50) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Total Number of Tubes In Bundle | MI_INSPBUND_TUBES01_N | Numeric | None |
Action This Inspection | MI_INSPBUND_ACTION_THIS_INSP_C | Character (50) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Tubes Plugged At Inspection Start | MI_INSPBUND_TUBES02_N | Numeric | None |
Tubes Plugged During This Inspection | MI_INSPBUND_TUBES07_N | Numeric | This column is not applicable if the value in the Action This Inspection column is NO ACTION. |
Tubes (Plugged At Start) Replaced | MI_INSPBUND_TUBES03_N | Numeric | This column is not applicable if the Action This Inspection column contains one of the following values:
|
Tubes (Not Previously Plugged) Replaced | MI_INSPBUND_TUBES04_N | Numeric | This column is not applicable if the Action This Inspection column contains one of the following values:
|
Bundle Inspection Summary | MI_EVENT_LNG_DSC_TX | Text | None |
Press_Test_Sub_Inspection Worksheet
On the Press_Test_Sub_Inspection worksheet, you can specify Pressure Test Sub-Inspection records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the Inspection Reference of the parent inspection specified on the Inspections worksheet. |
Pressure Test Inspection Reference | MI_EVENT_SUB_INSP_ID | Character (255) | Enter a unique value. Values in this column are used to identify the Pressure Test Sub-Inspection. |
Test Media - Shell Side | MI_INSPPTST_MEDIA_TEST_SH_C | Character (50) | None |
Test Media - Tube Side | MI_INSPPTST_MEDIA_TEST_TB_C | Character (50) | None |
Test Pressure -Shell Side | MI_INSPPTST_PRESS_TEST_SH_N | Numeric | None |
Test Pressure - Tube Side | MI_INSPPTST_PRESS_TEST_TB_N | Numeric | None |
Test Duration - Shell Side | MI_INSPPTST_DURATION_TEST_SH_N | Numeric | None |
Test Duration - Tube Side | MI_INSPPTST_DURATION_TEST_TB_N | Numeric | None |
Test Media Temperature - Shell Side | MI_INSPPTST_MEDIA_TEMP_SH_N | Numeric | None |
Test Media Temperature - Tube Side | MI_INSPPTST_MEDIA_TEMP_TB_N | Numeric | None |
No. of Gauges Used - Shell Side | MI_INSPPTST_NO_GAUGE_USED_SH_N | Numeric | None |
No. of Gauges Used - Tube Side | MI_INSPPTST_NO_GAUGE_USED_TB_N | Numeric | None |
Witnessed By - Shell Side | MI_INSPPTST_WITNESS_BY_SH_C | Character (255) | Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> |
Witnessed By - Tube Side | MI_INSPPTST_WITNESS_BY_TB_C | Character (255) | Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> |
SRV Set Pressure - Shell Side | MI_INSPPTST_SRV_SET_PRESS_SH_N | Numeric | None |
SRV Set Pressure - Tube Side | MI_INSPPTST_SRV_SET_PRESS_TB_N | Numeric | None |
Test Comments - Shell Side | MI_INSPPTST_COMMENTS_TEST_SH_T | Text | None |
Test Comments - Tube Side | MI_INSPPTST_COMMENTS_TEST_TB_T | Text | None |
General_Finding Worksheet
On the General_Finding worksheet, you can specify General Finding records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the values entered on the Inspections worksheet, if they exist. You can link multiple records to the same Inspection. |
Inspection Profile Category | MI_FIND_001_ITEM_PROFILE_CAT_C | Character (100) | A value is required. This column must only contain System Code IDs from the MI_INSPECTION_PROFILE_CATEGORY System Code Table. To verify which options are acceptable in your APM system, via Configuration Manager, refer to the appropriate table. The combination of values in the Inspection Profile Category, Inspection Profile Item, and Inspection Method Item columns must be unique. |
Inspection Profile Item | MI_FIND_001_ITEM_PROFILE_C | Character (100) | A value is required. The combination of values in the Inspection Profile Category, Inspection Profile Item, and Inspection Method Item columns must be unique. |
Inspection Method Item | MI_FIND_001_ITEM_METHOD_C | Character (100) | A value is required for each row. This column must only contain the System Code IDs from the MI_INSPECTION_METHOD_CATEGORY System Code Table. To verify which options are acceptable in your APM system, via Configuration Manager, refer to the appropriate table. The combination of values in the Inspection Profile Category, Inspection Profile Item, and Inspection Method Item columns must be unique. |
Sequence | MI_FIND_001_SEQUENCE_N | Numeric | None |
Location Details | MI_FIND_001_LOCATION_DETAILS_C | Text | None |
Headline | MI_FIND_001_HEADLINE_C | Character (50) | None |
Finding Summary | MI_FIND_001_SUMMARY_T | Text | None |
Type | MI_FIND_001_TYPE_C | Character (100) | This column must only contain the System Code IDs from the MI_FINDING_TYPE System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
As Found Degradation Mechanism |
MI_FIND_001_MECH_DET_C |
Character (100) |
This column must only contain the System Code IDs from the MI_DAMAGE_MECHANISM System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Damage Mode | MI_FIND_001_MODE_DET_C | Character (100) | This column must only contain the System Code IDs from the MI_DAMAGE_MODE System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Action Taken Code | MI_FIND_001_ACT_TAKEN_CODE_C | Character (100) | Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Action Taken Description | MI_FIND_001_ACT_TAKEN_DESC_T | Text | None |
Predictable | MI_FIND_001_PREDICTABLE_C | Character (3) | In the baseline APM system, This column must only contain the following System Code IDs:
The list in this field is populated by the MI_YES_NO System Code Table. If the system code table has been customized, the valid values could be different. To verify which options are acceptable in your APM system, via Configuration Manager, refer to the appropriate table. |
Custom_Sub_Inspection Worksheet
If you have created a custom sub inspection family, on the Custom_Sub_Inspection worksheet, you can specify the custom sub inspection records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_CMI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the values entered for the parent Inspection on the Inspections worksheet. You can link multiple records to the same Inspection. |
Sub Inspection Reference | MI_EVENT_SUB_INSP_ID | Character (255) | A value is required and must be unique. Values in this column are used to identify the custom sub inspection record. |
Family ID | FMLY_ID | Character (255) | A value is required and must match the value entered for the parent Inspection family on the Inspections worksheet. |
Inspection_Recommendation Worksheet
On the Inspection_Recommendation worksheet, you can specify Inspection Recommendation records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the values entered on the Inspections worksheet, if they exist. You can link multiple records to the same Full Inspection. |
Recommendation ID | MI_REC_ID | Character (255) | A value is required and must be unique. |
Target Completion Date | MI_REC_TARGE_COMPL_DATE_DT | Date | A value is required. Enter a value in the following format: YYYY-MM-DD hh:mm:ss
|
Recommendation Headline | MI_REC_SHORT_DESCR_CHR | Character (255) | None |
Recommendation Description | MI_REC_LONG_DESCR_TX | Text | None |
Recommendation Priority | MI_REC_PRIORITY_C | Character (50) | This column must only contain the System Code IDs from the MI_PRIORITY System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Required Equipment Status | MI_REC_REQUI_EQUIP_STATU_CHR | Character (50) | This column must only contain the System Code IDs from the MI_EQUIP_OP_STATE System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Business Impact | MI_REC_IMPAC_CHR | Character (100) | This column must only contain the System Code IDs from the MI_BUSINESS_IMPACT System Code Table. Refer to the (Picklist) worksheet for a list of values that you can enter in this column. |
Mandatory Date | MI_REC_MANDA_DATE_DT | Date | Enter a value in the following format: YYYY-MM-DD hh:mm:ss |
Assigned To Name | MI_REC_ASSIG_NM_CHR | Character (255) | Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> |
Author Name | MI_REC_AUTHO_NM_CHR | Character (255) | The value in this column must match an existing Security User who is assigned the Inspector, Inspection Administrator, or Inspection Supervisor Resource Role. Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> Note: If the Use State Management for Inspection Recommendations check box in Application Settings is selected, GE Vernova recommends removing this field from the worksheet. |
Reviewer Name | MI_REC_REVIE_NM_CHR | Character (255) | The value in this column must match an existing Security User who is assigned the Inspection Supervisor Resource Role. Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> Note: If the Use State Management for Inspection Recommendations check box in Application Settings is selected, GE Vernova recommends removing this field from the worksheet. |
Final Approver Name | MI_REC_FINAL_APPROVE_NAME_C | Character (255) | Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> |
Implemented Date | MI_REC_COMPL_DATE_DT | Date | Enter a value in the following format: <Last Name>, <First Name> ~ <User ID> |
Reference_Document Worksheet
On the Reference_Document worksheet, you can specify Reference Document records that you want to create or update.
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Equipment ID | MI_EQUIP000_EQUIP_ID_C | Character (255) | Values in this column must match the values entered on the Assets worksheet. You can link multiple records to the same asset. |
Functional Location ID | MI_FNCLOC00_FNC_LOC_C | Character (255) | Values in this column must match the values entered on the Functional_Location worksheet. You can link multiple records to the same Functional Location. |
CMMS System | MI_EQUIP000_SAP_SYSTEM_C MI_FNCLOC00_SAP_SYSTEM_C | Character (255) | Values in this column must match the values entered on the Assets or Functional_Location worksheet, if they exist. You can link multiple records to the same asset or Functional Location. |
Equipment Technical Number | MI_EQUIP000_EQUIP_TECH_NBR_C | Character (255) | Values in this column must match the values entered on the Assets worksheet, if they exist. You can link multiple records to the same asset. |
Inspection Reference | MI_EVENT_ID | Character (255) | Values in this column must match the values entered on the Inspections worksheet, if they exist. You can link multiple records to the same Full Inspection. |
Reference Document ID | CTIT_ID | Character (255) | A value is required and must be unique. |
Description | CTIT_DESC_TX | Character (255) | None |
Document Path | MIRD_DOC_PATH_CHR | Character (1023) | None |
About the Inspection Management (IM) Data Loaders Load Verification
Following a data load, you should perform the following steps in APM to confirm the integrity and accuracy of the data imported from the data loader workbooks:
- Access the details of the import job. These details will indicate if any errors, minor or otherwise, were encountered during the import job. The log may help account for any records that are unexpectedly absent after the data load.
- In Inspection Management or Record Manager, access the assets or Functional Locations specified in the data loader workbooks, and then verify that the expected Inspection Profiles, Inspection Methods, and Inspections are present or updated, and that any associated records that you expected to be created are also present in the database.