Schedule Jobs

About GAA Wind Scheduled Job Records

GAA Wind Scheduled Job records provide information about the schedule details that are used to import the Events data automatically for Sub Groups and generate Performance Report automatically for Sub Groups. A Scheduled Job can be configured to run as a one time job or as a recurring job.

Access a Scheduled Job

Procedure

  1. Access the GAA Wind Administrator page.
  2. Select the Schedule Jobs tab.
    A pane containing the list of Scheduled Jobs appears.
    Note: The first record is selected by default.
  3. Select the Scheduled Job that you want to access.
    The datasheet of the selected Scheduled Job appears.
    Important: You cannot update a One Time Scheduled Job if it has already run. Also, you cannot change the type of job schedule from One Time Scheduled Job to Recurring Scheduled Job or vice versa.
    Note: You can modify the values in the available fields, and then select Save to save your changes.

Create a Scheduled Job

Procedure

  1. Access the GAA Wind Administrator page.
  2. Select the Schedule Jobs tab.
    A pane containing the list of Scheduled Jobs appears.
    Note: The first record is selected by default.
  3. Select , and then select Event Import Job or Performance Report Job.
    A blank datasheet appears.
  4. As needed, enter values in the available fields.
    Note: You can create the following types of Event Import Scheduled Jobs:
    • One Time: This is a one-time job that is created based on the selected Import Duration Type. The Scheduled Job will start based on the selected Start Date. The following Import Duration Types are available:
      • Date range: Identifies the time period for which data will be imported. Event Import Start Date and Event Import End Date values are considered in Coordinated Universal Time (UTC) for importing the events data.
      • Month and Year: Identifies the month and year for which data will be imported.
    • Recurring: This is a recurring job based on the selected Repeat Interval, Start Date, and End Date. Import Start Date indicates the start date from when the event data must be imported. Import End Date is based on the selected Repeat Interval.
    Note: You can create the following types of Performance Report Scheduled Jobs:
    • One Time: This is a one-time job that is created to generate performance reports for the selected month and year. The Scheduled Job will start based on the selected Start Date.
    • Recurring: This is a monthly recurring job based on the selected Start Date and End Date. Month and Year indicates the start month and year from when the performance report is generated. Every occurrence of the job will generate performance reports for the next month from the previous occurrence.
    Important: If the Overwrite Existing Data box is cleared, and data exists for the selected date range or month and year, then the Scheduled Job will not create new records. For a Sub Group, you can create multiple One Time Scheduled Jobs, but only one Recurring Scheduled Job.
  5. Select Save.
    The Scheduled Job is created.

Delete a Scheduled Job

Procedure

  1. Access the GAA Wind Administrator page.
  2. Select the Schedule Jobs tab.
    A pane containing the list of Scheduled Jobs appears.
  3. In the pane, select the Scheduled Job that you want to delete.
  4. Select Delete.
    The Delete Schedule Job window appears, asking you to confirm that you want to delete the selected item.
  5. Select Yes.
    The Scheduled Job is deleted.