Reliability Analytics Upgrade

Upgrade or Update Reliability Analytics to V5.0.0.0.0

Upgrading or updating to the V5.0.0.0.0 is a two-step process. You need to first upgrade to GE Digital APM V4.6.2.0.0 or later and then follow the steps to upgrade or update to V5.0.0.0.0.

The following table provides you the reference to procedures to upgrade from an earlier GE Digital APM version to the latest version.

Upgrade from Upgrade to Procedure
V4.6.0.0.0 through V4.6.3.0.0V5.0.0.0.0Upgrade from any version V4.6.0.0.0 through V4.6.3.0.0

Upgrade from any version V4.6.0.0.0 through V4.6.3.0.0

The following tables outline the steps that you must complete to upgrade this module to V5.0.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

StepTaskNotes
1Ensure that the Meridium Simulation Service is installed and running.If the basic GE Digital APM system architecture is already installed, the Meridium Simulation Service is automatically installed and run.
2Revert the following query to baseline to view the Recommendation chart on the RA Overview page:
  • Public\Meridium\Modules\Reliability Manager\Queries folder:
    • Dashboard - Recommendation Summary
This step is required only if you have previously modified the query. Otherwise, this step will be completed automatically when you upgrade the components in the basic GE Digital APM system architecture.
To revert queries to baseline:
  1. Access the Catalog page.
  2. Navigate to the Public folder for the query that you want to revert: Public/Meridium/Modules/<module name>/Queries
  3. Select the check box next to the query that you want to revert, and then select .

    The Confirm Delete window appears, asking you to confirm if you want to delete the selected query.

  4. Select OK. The selected query is deleted.
  5. Navigate to the module-specific Baseline folder for queries: Baseline/Meridium/Modules/<module name>/Queries
  6. Select the check box next to the query that you want to revert, and then select .

    The Catalog Folder Browser window appears.

  7. Navigate to the folder containing the public query that you deleted in step 3.
  8. Select OK.

    A message appears, indicating that the selected item has been copied successfully.

  9. Repeat steps 2-8 for each query that you want to revert to baseline.