Asset Health Manager Upgrade
Upgrade or Update Asset Health Manager to V5.0.0.0.0
Upgrading or updating to the V5.0.0.0.0 is a two-step process. You need to first upgrade to GE Digital APM V4.6.2.0.0 or later and then follow the steps to upgrade or update to V5.0.0.0.0.
The following table provides you the reference to procedures to upgrade from an earlier GE Digital APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V4.6.0.0.0 through V4.6.3.0.0 | V5.0.0.0.0 | Upgrade from any version V4.6.0.0.0 through V4.6.3.0.0 |
Upgrade from any version V4.6.0.0.0 through V4.6.3.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.0.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Upgrade from PDI to OT Connect | This step is required only if you are using Content Map records as health indicators sources. |
2 | Optional:
Resync Health Indicators Depending on the status of potential health indicator sources in your database, the resync will result in one or both of the following scenarios:
| This step is optional. |