OT Connect Services
Install OT Connect Adapter Service
Before You Begin
OPC Classic DA and HDA
You must perform the following steps to install the 64-bit OPC Core Components on the OT Connect Process Data server:- On the machine that will serve as the OT Connect Process Data Server, access the GE Digital APM distribution package, and then navigate to the \V4.4.0.0_3rd_Party_Software\OPC Core Components folder.
- Ensure that all the OPC servers or clients on the Process Data server are stopped to avoid conflicts with common libraries used by both 32-bit and 64-bit OPC Core Components.
- Double-click on OPC Core Components Redistributable (x64) 3.00.108.msi.
- Select I Agree to accept the license.
- Select Next on the following windows to accept the default selections, and install the software.
- Close the installer.
About This Task
Procedure
Configure OT Connect Adapter Service
About This Task
You can make the modifications by opening the file in an application that can modify JSON text (for example, Notepad). The following instructions provide details on making all required modifications at one time using the text editor.
Note: This configuration file defines several endpoints on the GE Digital APM Server with URLs and ports that must be accessible from the OT Connect Process Data Server. Ensure that your firewalls are configured to allow this access.
Procedure
Install OT Connect Conductor Service
About This Task
Note: Re-installing the OT Connect Conductor Service will reset its appsettings.json to the default settings.