General Reference
OT Connect System Requirements
License Requirements
The APM OT Connect license is required to take full advantage of the OT Connect functionality.
Additional Components Required
In addition to the basic GE Digital APM system architecture, your system must also contain the following components:
- OT Connect Conductor service must be installed on the GE Digital APM Server.
- OT Connect Process Data Server: A machine on which the OPC compliant software is installed. The software requirements of this server are determined by the third-party distributor of the software. OT Connect Adapter must be installed on the OT Connect Process Data Server.
- Process Historian: A machine on which the process historian software is installed. The software requirements of this machine are determined by the third-party distributor of the software.
Refer to the supported software and devices documentation for information about OT Connect Process Data Servers and Process Historians that are tested for the OT Connect feature. The OT Connect Adapter can be installed and run on the OT Connect Process Data Server in OT Source Capability Utility mode to validate the capabilities of specific OT Connect Process Data Servers and process historians on a case-by-case basis. Refer to the deployment section for more information on the OT Connect Adapter.
System Architecture
The following image shows the basic system architecture for deploying OT Connect with one GE Digital APM Server.
Deploying OT Connect
After you have installed and configured the basic GE Digital APM system architecture, you must perform some configuration steps specifically for OT Connect.
If you want to use OT Connect with Asset Health Manager and Policy Designer, you must also configure the services associated with these modules.
OT Connect System Architecture

The Conductor requires access to the GE Digital APM Datasource(s), so it should be installed on the GE Digital APM Server with the other services.
Each OT Connect Adapter Service can connect a single Process Historian or OPC Server to a single GE Digital APM Datasource, so your solution may require multiple OT Connect Adapter Services, installed on the same or different servers.
The OT Connect Adapter Service does not require any inbound connections, only outbound connections to the Message Broker and Cache services, allowing the OT Connect Process Data Server to be deployed within a DMZ or OT Network without compromising security.
Required Server Ports
To ensure successful communications between GE Digital APM and OT Connect, make sure the listed ports are open.
Feature | Firewall Port | From | To |
---|---|---|---|
Tag and Subscription Synchronization |
Configurable; 1433 for a default SQL Server. Additional ports as required by the chosen Authentication scheme | OT Connect Conductor | APM Database |
Tag and Subscription Synchronization | Configurable; 6379 by default | OT Connect Conductor | Redis Server |
Tag and Subscription Synchronization | Configurable; 61616 by default | OT Connect Conductor | ActiveMQ Server |
All connectivity for that OT Source | Configurable; 6379 by default | OT Connect Adapter | Redis Server |
All connectivity for that OT Source | Configurable; 61616 by default | OT Connect Adapter | ActiveMQ Server |
Data Model

OT Source: Source of Tags and Tag Value from the Edge
The following table provides a list and description of the fields that exist in the OT Source family and are available on the baseline OT Source datasheet. The information in the table reflects the baseline state and behavior of these fields. If your implementation has been customized, these fields may behave differently, and fields in addition to those listed here may be available.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Site Filtering section of the documentation.
Field Caption/ID | Data Type | Description | Behavior and Usage |
---|---|---|---|
MI_OTSRC_ID_C | Character | Unique Identifier | None |
MI_OTSRC_CONN_DEF_T | Text | Connection Configuration | Reserved for future use |
MI_OTSRC_TYPE_C | Type | Text |
This field is a selection from a predefined list. Options include OPC HDA and Simulation |
MI_OTSRC_NAME_C | Character | Name | None |
MI_OTSRC_LAST_UPDT_D | Date | Last Update Time | None |
MI_OTSRC_LAST_SYNC_D | Date | Last Sync Time | None |
MI_OTSRC_SYNC_RATE_N | Numeric | Minutes between Tag Synchronizations | None |
MI_OTSRC_CAPABILITY_N | Numeric | Capability | Bit Flags |
MI_OTSRC_SYNC_DEF_T | Text | Synchronization Configuration | JSON |
MI_OTSRC_SUB_RATE_N | Numeric | Default Subscription Rate | None |
Source Tag: Tag definition from Source on the Edge
The following table provides a list and description of the fields that exist in the Source Tag family and are available on the baseline Source Tag datasheet. The information in the table reflects the baseline state and behavior of these fields. If your implementation has been customized, these fields may behave differently, and fields in addition to those listed here may be available.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Site Filtering section of the documentation.
Field Caption/ID | Data Type | Description | Behavior and Usage |
---|---|---|---|
MI_SRCTAG_ID_C | Character | Unique Identifier | None |
MI_SRCTAG_NAME_C | Character | Name | Unique name in Process Historian |
MI_SRCTAG_DESC_C | Character | Description | |
MI_SRCTAG_ITEM_C | Character | - | Reserved for future use |
MI_SRCTAG_COMMENTS_T | Text | Comments | |
MI_SRCTAG_UOM_C | Character | UoM | Reserved for future use |
MI_SRCTAG_RAW_UOM_C | Character | Raw UoM | UoM string reported by Process historian |
MI_SRCTAG_EXT_PROPS_T | Text | Extended Properties | |
MI_SRCTAG_DELETED_B | Boolean | This Tag was deleted from the OT Source | |
MI_SRCTAG_DATA_TYPE_C | Character | Data Type |
This field is a selection from a predefined list. Options include Boolean, Integer, Decimal, String, Timespan, DateTime |
MI_SRCTAG_HS_OTSRC_FK_N | Numeric | OT Source Entity Key | Foreign Key to OT Source Records family |
MI_SRCTAG_MIGR_FMLY_KEY_C | Character | Migrated Tag Family Key | Used for upgrade from MI_TAG based families (OPC Tag, GE Tag, AMS Tag) |
MI_SRCTAG_MIGR_ENTY_KEY_C | Character | Migrated Tag Entity Key | Used for upgrade from MI_TAG based families (OPC Tag, GE Tag, AMS Tag) |
Content Map: The relationships between content and sources
The following table provides a list and description of the fields that exist in the Content Map family and are available on the baseline Content Map datasheet. The information in the table reflects the baseline state and behavior of these fields. If your implementation has been customized, these fields may behave differently, and fields in addition to those listed here may be available.
Field Caption/ID | Data Type | Description | Behavior and Usage |
---|---|---|---|
MI_CONTMAP_ID_C | Character | Unique Identifier | None |
MI_CONTMAP_TMPLT_NAME_C | Character | - | Reserved for future use |
MI_CONTMAP_UOM_C | Character | UoM | Reserved for future use |
MI_CONTMAP_LMT_DEFS_T | Text | Limit Definitions | JSON |
MI_CONTMAP_TRIGGER_B | Boolean | - | Reserved for future use |
MI_CONTMAP_REQ_CAP_N | Numeric | OT Source Capabilities Required by this Content | Bit flags |
MI_CONTMAP_EQUIP_FK_N | Numeric | Equipment Key | Foreign Key to Equipment Record |
MI_CONTMAP_FLOC_FK_N | Numeric | Functional Location Key | Foreign Key to Functional Location Record |
MI_CONTMAP_SRCTAG_FK_N | Numeric | Source Tag Key | Foreign key to Source Tag record |
MI_CONTMAP_PLCY_INST_FK_N | Numeric | Policy Instance Key | Foreign Key |
Security Groups and Roles
The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned.
Security Group | Roles |
---|---|
MI OT Connect Administrator |
MI OT Connect Admin MI Health Admin |
MI OT Connect Viewer |
MI Health User MI Health Power MI OT Connect User |
MI Content Template User |
MI Health Admin MI OT Connect Admin |
MI Content Template Viewer |
MI Health User MI Health Power MI OT Connect User |
The baseline family-level privileges that exist for these Security Groups are summarized in the following table.
Family | MI OT Connect Administrator | MI OT Connect Viewer |
---|---|---|
OT Source | View, Update, Insert, Delete | View |
Source Tag | View, Update, Insert, Delete | View |
Family | MI Content Template User | MI Content Template Viewer |
---|---|---|
Content Map | VIEW, INSERT, UPDATE, DELETE | View |
Site Filtering
The OT Source family uses the GE Digital APM Site Filter Control. When an OT Source record is created, it is assigned as Global. If the record is not reassigned to a specific site, then the user will always see the global record. For more information, refer to the Site Filtering section of the documentation.
The OT Source is used to facilitate the transfer of records from your Process Historian server into GE Digital APM. Specifically, Source Tags are transferred into GE Digital APM. The records that are associated with the data source are assigned to Global when they are initially transferred into GE Digital APM.
The content Maps are foundational records that are used to map Source Tags to Equipment, Functional Locations, Health Indicators, and/or Policy Instances. The content Maps will inherit the site of the asset within the record.