Ensure that the Equipment ID or the Functional Location ID fields in the Instrumented Function datasheet are populated with the values that correspond to the Asset that is being protected by the Instrumented Function.
The Health Summary page for the Asset appears, displaying the health indicators for the Asset.
Note: If there is no value in the Equipment ID or the Functional Location ID fields of the Instrumented Function, then the button is disabled.
Note: Policies and other health indicator sources can be leveraged to provide a holistic view of the asset which include but are not limited to the following: