Instrumented Function records store details about a specific function of a safety instrumented system. This topic provides an alphabetical list and description of the fields that exist for the Instrumented Function family. The information in this table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Abnormal State |
Character |
A short description of the specific abnormal state of the operation. |
This field does not appear on the datasheet. |
Availability Target | Number | The percentage of time that the instrumented function must be operational. | Provide a value between 0 and 100. This value is compared with the availability of a Protective Instrument Loop to determine if the loop meets the availability target. |
Concurrent Safe State Hazard |
Text |
A description of the hazardous event that could occur if the safe state associated with the instrumented function occurs simultaneously with the safe state of a different instrumented function. |
This field appears on the Concurrent Safe State Hazard datasheet without a field caption, and a value is set by default. You can remove this value and enter your own value. |
Concurrent Safe State Hazard? | Logical | Indicates whether the safe state associated with the instrumented function can cause a hazardous event if it occurs concurrently with the safe state of a different instrumented function. | This field appears on the Concurrent Safe State Hazard datasheet, which you can select to indicate that the safe state for the instrumented function can lead to a hazardous event if that safe state occurs simultaneously with the safe state of a different instrumented function. |
Consequence Description | Text | A description of the risk that is associated with the hazardous event that exists in the Hazardous Event field. | If the value in the SIL Assessment Method field is PHA - Internal, after you select a Risk Assessment record from a Hazards Analysis, this field is populated with the value in the Consequence Description field in the Hazards Analysis Consequence record that is linked to the Risk Assessment record you selected. |
Demand Rate (Source) | Character | The demand rate for the instrumented function (i.e., Low demand or High demand). | This field appears on the Safety Requirement Specification datasheet, and contains the text Low Demand by default. You can modify this value. |
Equipment ID | Character | The ID of the Equipment that you want to link to the Instrumented Function. | On the datasheet, this field contains a |
Equipment Key | Number | The Entity Key of the Equipment that is linked to this Instrumented Function. | The GE Digital APM system uses this value to populate the Equipment ID field that appears on the Instrumented Function datasheet. |
Failure Rate UOM | Character | The unit of measure that is associated with the value in the Required Probability of Failure field. | This field contains
the following values:
|
Frequency of Initiating Event (Per yr) | Number | The number of times per year that the initiating event occurs. | If the value in the SIL Assessment Method field is PHA - Internal, after you select a Risk Assessment record from a Hazards Analysis, this field is populated with the value in the Cause Frequency (per year) field in the Hazards Analysis Cause record that is linked to the Hazards Analysis Consequence record that is linked to the Risk Assessment record you selected. |
Function Type | Character | The type of the instrumented function. | This field contains a list with
the following baseline values:
|
Functional Location ID | Character | The ID of the Functional Location that is linked to the Instrumented Function. | On the datasheet, this field a |
Functional Location Key | Number | The Entity Key of the Functional Location that is linked to this Instrumented Function. | The GE Digital APM system uses this value to populate the Functional Location ID field. |
Hazardous Event | Character | A description of the event for which the instrumented function exists to prevent or mitigate risk. | If the value in the SIL Assessment Method field is PHA - Internal, after you select a Risk Assessment record from a Hazards Analysis, this field is populated with the value in the Consequence Type field in the Hazards Analysis Consequence record that is linked to the Risk Assessment record you selected. |
Hazards Analysis Date | Date | The date the Hazards Analysis to which this Instrumented Function is linked was last modified. | On the datasheet, this field is disabled and populated automatically with the value stored in the Last Modified Date field in the Hazards Analysis that is linked to this Instrumented Function and whose ID appears in the Hazards Analysis Reference field. |
Hazards Analysis Reference | Character | The ID of the Hazards Analysis that is linked to this Instrumented Function. | This field does not appear on the datasheet. |
Hazards Analysis Reference Key | Number | The Entity Key for the Hazards Analysis that is linked to this Instrumented Function. | This field is used by the GE Digital APM system to populate this Instrumented Function record with information from the Hazards Analysis that is linked to this Instrumented Function. |
Initiating Event | Character | A short description of the initiating event whose description exists in the Initiating Event Description field. | If the value in the SIL Assessment Method field is PHA - Internal, after you select a Risk Assessment record from a Hazards Analysis, this field is populated automatically with the value in the Cause Type field in the Hazards Analysis Cause record that is linked to the Hazards Analysis Consequence record that is linked to the Risk Assessment record you selected. |
Initiating Event Description | Text | A description of the event which could initiate a series of events that present the risk whose description exists in the Consequence Description field. | If the value in the SIL Assessment Method field is PHA - Internal, after you select a Risk Assessment record from a Hazards Analysis, this field is populated automatically with the value in the Cause Description field in the Hazards Analysis Cause record that is linked to the Hazards Analysis Consequence record that is linked to the Risk Assessment record you selected. |
I/O Functional Relationship Details | Text | A description of the relationship between the inputs and outputs for the process, including details such as logic and mathematical functions. | This field appears on the Safety Requirement Specification datasheet. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Maintenance and Test Requirements | Text | A description of the requirements for maintenance and testing procedures for the instrumented function. | This field appears on the Safety Requirement Specification datasheet, and a value is set by default. You can remove this value and enter your own values. |
Maintenance Override | Logical | A logical field that stores the value True or False and indicates whether the process requires override procedures for maintenance activities. | By default, this field does not appear on the datasheet. |
Manual Shutdown | Logical | A logical field that stores the value True or False and indicates whether the process requires manual shutdown. | By default, this field does not appear on the datasheet. |
Max Process Variable | Number | A number representing the upper value for the process variable range. | This field appears on the Safety Requirement Specification datasheet. This value combined with the value stored in the Min Process Variable field make up the process variable range. |
Min Process Variable | Number | A number representing the lower value for the process variable range. | This field appears on the Safety Requirement Specification datasheet. This value combined with the value stored in the Max Process Variable field make up the process variable range. |
Normal Operation Mode | Text | A description of the normal operating mode for the instrumented function. | By default, this field appears on the Safety Requirement Specification datasheet and a value is set. You can remove this text and enter your own values. |
Operation Mode Description | Character | The description of the abnormal mode of operation. | This field appears on the Safety Requirement Specification datasheet and is enabled only if the value for the Operation Modes field is ABNORMAL. If the value in the Operation Modes field is NORMAL, this field is disabled. |
Operation Modes | Character | The mode of operation for the instrumented function. | This field appears on the Safety Requirement Specification datasheet and contains
the following values:
|
Operator Interface Requirement | Text | A description of the Operator Interface requirements. | This field appears on the Safety Requirement Specification datasheet, and a value is set by default. You can remove this text and enter your own values. |
PIF Description | Character | Stores a description of the instrumented function. | On the datasheet, this field appears as a text box labeled IF Description, in which you can enter your own value. |
PIF ID | Character | An ID for the instrumented function. | On the datasheet, this field appears as a text box labeled IF ID, in which you can enter your own value. This value will appear in the list of Instrumented Functions on the left pane on the SIL Analysis Summary page. This field is required. |
Pre Alarm | Number | A number representing the point on the process variable range at which the pre-alarm should be triggered. | This field appears on the Safety Requirement Specification datasheet. |
Process Service Description | Text | A description of the specifications for the process service. | This field appears on the Safety Requirement Specification datasheet. |
Process Speed | Number | A number representing the time in seconds that the process for which the instrumented function takes to complete. | None |
Required Probability of Failure | Number | A number that represents the target probability that an instrumented function failure will occur. |
|
Required SIF Action | Text | A description of the action that the instrumented function performs in response to a triggered alarm. | This field appears on the Safety Requirement Specification datasheet. |
Reset Requirement | Text | A description of the requirements for resetting a process after it has been tripped. | This field appears on the Safety Requirement Specification datasheet and a value is set by default. You can remove this text and enter your own value. |
Response Time | Number | A numeric value that represents the time in seconds that it takes for the instrumented function to respond to the initiating event and bring the process to a safe state. | None |
Risk Reduction Factor (RRF) | Number | A number representing the factor by which the risk should be reduced for the instrumented function. | If the value in the SIL Mode field is Low Demand and the value in the SIL Assessment
Method field is Layer of Protection Analysis - Internal or Risk Matrix - Internal,
this field is disabled and populated automatically with the inverse of the value
in the Required Probability of Failure field. For all the other SIL Assessment methods, when the value in the SIL Mode field is Low Demand and the value in the SIL Assessment Method field is not Layer of Protection Analysis - Internal or Risk Matrix - Internal, this field is enabled and you can type a value directly into the Risk Reduction Factor field. Note that:
|
Safe State Description | Text | A description of the safe state to which the process should be taken via the instrumented function. | None |
Selected SIL Level | Number | A number representing the SIL value that is required for the instrumented function. | On the datasheet, this field is disabled and populated automatically if the value
in the SIL Assessment Method field is anything other than External. If the SIL Assessment Method field contains an External value, this field is enabled and appears as a list that is populated with values from the MI SAFETY INDEX LEVEL System Code Table. You can select a value from the list. If a value exists in the Required Probability of Failure field and you try to delete the value in the Selected SIL Level field, an error message appears, and you will not be able to delete the value. |
SIL Analysis Key | Number | The Entity Key of the SIL Analysis to which the Instrumented Function is linked. | This field is used internally by the GE Digital APM system. |
SIL Assessment Method | Character | The method used to assess the risk that is associated with the instrumented function. | This field contains the following values:
|
SIL Mode | Character | The SIL mode that is defined for this instrumented function. | This field contains the
following baseline values:
|
SIS System ID | Character | The ID of the Logic Solver to which the Instrumented Function is linked. | On the datasheet, this field appears as a list labeled SIS ID and contains the values
that exist in the SIS ID field in the Logic Solvers that are
linked to the SIL Analysis with which you are currently working. If a logic solver has been set as default, then the ID of the same logic solver is populated in the SIS System ID field. |
Site Description | Character | A description of the site that is specified in the Site ID field. | None |
Site ID | Character | The ID of the site that is associated with the instrumented function. | On the datasheet, this field is disabled and populated automatically with the value in the Site ID field of the associated SIL Analysis. |
Spurious Trip Limit (per yr) | Number | A number representing the number of times per year it is acceptable for a spurious trip to occur for this instrumented function. | This value is used to determine the value in the Meets STR Limit field in a Protective Instrument Loop that is linked to the Instrumented Function. |
Startup And Restart Procedure | Text | A detailed description of the start up and restart procedures for the process. | This field appears on the Safety Requirement Specification datasheet and a value is set by default. You can remove this text and enter your own value. |
Survival Requirement | Text | A description of the requirements for the instrumented function to survive a catastrophic event, such as an earthquake. | This field appears on the Safety Requirement Specification datasheet and a value is set by default. You can remove this text and enter your own value. |
Trip Mode | Character | A short description of the trip mode (i.e., energize to trip or de-energize to trip). | This field appears on the Safety Requirement Specification datasheet and the value is set to de-energize to trip by default. You can remove this value and enter your own value. |
Trip Point | Number | A number representing the point on the process variable range at which the trip alarm should be triggered. | This field appears on the Safety Requirement Specification datasheet. |
Unit Description | Character | A description of the unit that is specified in the Unit ID field. | None |
Unit ID | Character | The ID for the unit where the instrumented function exists. | You can enter your own value. |
UOM | Character | Units of measure for values such as Trip Point, Min Process Variable, Max Process Variable, Pre-alarm. | None |
Copyright © 2018 General Electric Company. All rights reserved.