To indicate the progress a user makes while entering readings on a Route, Rounds Data Collection displays a progress bar indicating the percentage of a Route for which you have entered readings as well as the number of checkpoints for which you have entered readings on a Route.
This progress bar appears in the following places:
This progress bar only tracks the progress of an individual user or device on a Route. In other words, the progress bar is not synchronized among multiple users and devices.
Consider a Route with 60 checkpoints. If one user enters 20 readings on that Route, the progress bar indicates that the Route is 30% complete. If another user then accesses the same Route, this second user does not see that the Route is 30% complete. Instead, this user sees that there are 40 checkpoints remaining on the Route, and 0% of those 40 checkpoints has been completed.
Copyright © 2018 General Electric Company. All rights reserved.