You can create the following types of recommendations in Rounds Data Collection:
New Recommendation: This Rounds recommendation is linked to the checkpoint. Create this recommendation if you want to provide suggestions on the checkpoint. The information about the checkpoint and the asset linked to it is populated on the datasheet for the recommendation.
Standalone Recommendation: This Rounds recommendation is linked to the asset that is associated with the checkpoint. Create this recommendation if you want to provide suggestions on the asset that is linked to that checkpoint. The information of only that asset is populated on the datasheet for the recommendation. The information about the checkpoint is not populated. Standalone recommendations do not appear in the Recommendations pane of a Route. They only appear in the Recommendations section on the RDC Overview page.