When you scan a barcode or RFID tag, you will be navigated automatically to the checkpoint associated with that barcode or RFID tag. You can, however, temporarily disable this navigation and enable the Copy Scan feature instead. On a Windows Mobile Device, you can use the Copy Scan feature to paste a scan ID value into a reading or recommendation when you scan the barcode or RFID tag.
For example, assume you are creating a recommendation for an piece of equipment, and you want to include the scan ID for the piece of equipment in the recommendation. Instead of manually typing the ID value, you can use the Copy Scan feature to populate the recommendation automatically with the scan ID.
Steps
On the Options menu or at the bottom of the screen, select Copy Scan.
Copyright © 2018 General Electric Company. All rights reserved.