Create a Recommendation from a Reading on a Windows Mobile Device

Steps

  1. Access Rounds on a Windows mobile Device.

  2. On the Home screen, select View Routes.

    The Routes screen appears, displaying the Route records that were last downloaded.

  3. Select the Detail View button.

    The Readings - Detail screen appears.

  4. On the Readings - Detail screen, select .

    The New Recommendation screen appears.

    The following text boxes are populated automatically with values from the reading:

  5. If the Measurement Location record that is associated with this Operator Rounds Recommendation record contains a value in the Asset Description box, that value will appear below in the Asset ID box.

  6. In the Headline box, enter a headline for the recommendation.
  7. In the Description box, enter a description of the recommendation.

    Note: If you entered text in the Description box on the Readings - Detail screen, that text will appear in the Description box on the New Recommendation screen. You can modify the description on this screen, and the updated text will be displayed when you return to the Readings - Detail screen.

  8. In the Priority list, select a priority for the recommendation. You can select: High, Medium or Low.

  9. Select Save.
  10. The recommendation is saved, and the Readings - Detail screen returns to focus.

Copyright © 2018 General Electric Company. All rights reserved.