Rounds Sequence Information Records

Rounds Sequence Information records store information about the order in which checkpoints appear in a route. This information is used when downloading Routes to a Windows Mobile handheld device.

Note: The values in Rounds Sequence Information records cannot be modified in Record Manager. These records are created or updated automatically to reflect the order in which checkpoints are arranged within a route in Rounds Designer. Records are created or updated when you select Save Route Sequence, after the Rounds Designer page has been closed, or on a defined schedule.

This topic provides an alphabetical list and description of the fields that exist for the Rounds Sequence Information family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Checkpoint or Condition Key

Numeric

The Entity Key of the checkpoint or condition for which this record was created.

This field is populated automatically.

Root Level Parent Key

Numeric

The Entity Key of the Route containing the checkpoint.

This field is populated automatically.

Route Key

Numeric

The Entity Key of the Route containing the checkpoint.

This field is populated automatically.

Sequence

Numeric

The position the checkpoint appears in a Route.

This field is populated automatically.

Copyright © 2018 General Electric Company. All rights reserved.