Note: You cannot use either drag-and-drop method with touch interfaces. When using a touch interface, you must reorder nodes within a Route by changing the order number.
Tip: You can select to open a menu that includes options to expand or collapse all checkpoints, allowing you to reorder routes more easily.
In the left pane, select the button next to the node whose order you want to change, drag it to the Node Pin Board pane, and then drop it.
The node is grayed out in its original location in the left pane.
Hint: You can repeat this step to move as many nodes to the Node Pin Board as required to complete the reordering operation. Nodes can be left on the Node Pin Board while you compete other tasks on the Route.
In the left pane, navigate to the new location where you want the node to appear.
In the Node Pin Board pane, next to each node that you want to move, select the check box.
The drag feature is enabled.
Select the button next to one of the nodes in the Node Pin Board pane, drag the node to the left pane, and drop it in the new location.
Hint: A blue insertion marker will appear when the node placeholder is positioned at a location where it can be dropped.
A confirmation dialog appears, noting the number of first-level measurement locations and checkpoint conditions that will be dropped into the Route.
Select Yes.
The node is reordered.
To make the new Route sequence available immediately for Windows Mobile handheld devices, select the route level, and then select Save Route Sequence.