Operator Rounds Recommendation records are created by mobile device users to communicate maintenance or follow-up inspection requirements based on the observed conditions of checkpoints on a Route. Recommendations can be created linked to a specific checkpoint and the related asset, or as standalone recommendations that are linked to the Equipment or Functional Location only.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Note: When configuring offline forms, be careful to include only fields where field level rules are not used. In particular, fields that are required and disabled should be avoided. In many cases, field level rules may be replaced by field behaviors, which are supported in offline forms.
This topic provides an alphabetical list and description of the fields that exist for the Operator Rounds Recommendation family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive; instead, it is limited to field behavior that differs from General Recommendation fields.
Field |
Data Type |
Description |
---|---|---|
Assigned To | Text | The user to which the recommendation is assigned. This field appears in the Recommendations section of the RDC Overview page. |
Created from Measurement Location | Character | The Measurement Location for which the recommendation was created. |
Created from Measurement Location Asset | Numeric | The asset that is associated with the Measurement Location for which the recommendation was created. |
Created On | Date | The date and time on which the recommendation was created. This field appears in the Recommendations section of the RDC Overview page. |
Description |
Text | The text that appeared in the Description cell when the Recommendation was saved on the mobile device. |
Headline | Text | The text that appeared in the Headline cell when the Recommendation was saved on the mobile device. |
Measurement Location Entity Key | Numeric | The Entity Key of the Measurement Location for which the recommendation was created. |
Recommendation ID | Numeric |
A value that identifies the recommendation record. |
Source ML Description | Text | For recommendations, other than standalone recommendations created on a mobile device, this field is populated automatically with the value that is stored in the ML or LR Description field in the Measurement Location or Lubrication Requirement record for which the recommendation was created. |
Type | Text | The type of recommendation (e.g., Operator Rounds Recommendation). This field appears in the Recommendations section of the RDC Overview page. This field is populated automatically. |
Copyright © 2018 General Electric Company. All rights reserved.