Lubrication Component records store information about lubrication components and provide values for drop-down lists used in the Lubrication Requirement and Lubrication Requirement Template families. This topic provides an alphabetical list and description of the fields that exist for the Lubrication Component family and appear on the Lubrication Component datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Component Sub Type |
Character |
The sub type of a lubrication component type. |
The values in this field populate the Component Sub-Type lists on Lubrication Requirement and Lubrication Requirement Template datasheetes. |
Component Type | Character | The type of lubrication component. |
Organizes records in the Lubrication Component family into distinct groups. The values in this field populate the Component lists on Lubrication Requirement and Lubrication Requirement Template datasheets. |
Description | Character | The description of the lubrication component type or sub type. | If there is a value in the corresponding Component Sub Type field, then the value in this field is a description of the Component Sub Type. However, if the corresponding Component Sub Type field is empty, then the value in this field is a description of the Component Type. |
ID | Character | A unique value that identifies the lubrication component. | This field is required and must be unique. |
Copyright © 2018 General Electric Company. All rights reserved.